Three Methods of Operation

You can operate the E5072A using one of three operating methods: using keys on the front panel, using a mouse and keyboard, and using the touch screen. This section illustrates these three operating methods through the example in which the channel window layout is set to the four-channel display as shown in the following figure.

In the next section and those following it, a series of operations is expressed as follows:

Display > Allocate Traces >  

Four-Trace Display

Operating Method Using Keys

  1. Press the DISPLAY key in the RESPONSE Block.

  1. Press or key to move the cursor to the Allocate Traces, then press Enter or ()  key.

  1. Press or key to move the cursor to , then press Enter key.

Operation Method Using a Mouse

  1. From the Response menu, press Display key.


     

  1. Click Allocate Traces.

  1. Click

Operation Method Using the Touch Screen

  1. Press Display key after presetting the E5072A (Executing Preset).

  1. Click/Press Allocate Traces.

  1. Click/Press any desired setting.