Change Date/Time Settings

The E5072A has the built-in clock that keeps track of the date and time. This clock is used for the following functions.

Below are the options to change the Date & Time of E5072A:

For windows 7, the administrator password is required to change the time and date setting when login as standard user.

Other topics about Using Windows