Requirements for operating the MWA software are as follows:
OS: Windows 7
Microsoft Excel 2010/2013
The back-end application of the MWA must be installed.
Note: The MWA operates only when the number of channels is three or more (four or more for the VNA settings).
If you wish to make multiport measurements, the following multiport test set are supported by the MWA.
The option 020 (E5092A-020).
Configurations of E5092A 13-port, 16-port, 22-port and X-10-port crossbar are supported by the MWA for the E5092A-020.
Note: Up to two multiport test set can be used.
When using the ECal module with calibration wizard in the back-end application of the MWA, the 4-port ECal module supported by the VNA is required. Refer to ECal for supported ECal modules by the VNA.