Applicable Models: M937xA, P937xA (Read-Write) Sets the logic of the index line ("Trig Out" port) on the last PXIe module. There is no soft front-panel element for this feature. |
|
Parameters |
|
<char> |
Choose from: POSitive - Causes the Index line to have positive logic (Low signal indicates that the measurement is complete) NEGative - Causes the Index lines to have negative logic (High signal indicates that the measurement is complete). |
Examples |
CONT:HAND:EXT:INDEX:LOG POS control:handler:ext:index:logic negative |
Query Syntax |
CONTrol:HANDler:EXT:INDex:LOGic? |
Return Type |
Character |
POSitive |