This VB Script example creates and calibrates a scalar mixer measurement.
To run this example without modification you need the following:
An ECal module that covers the frequency range of the measurement.
A power meter must be available to the VNA. This can be accomplished either by attaching the meter to the VNA via a GPIB cable, or by using SCPI over LAN.
By removing the comments ( ' ) at the start of the BLUE code, it can also do the following:
Load a mixer setup file
Use ECal characterizations
Specify Mechanical Cal Kits
Perform manual ECal orientation.
Specify the thru measurement method.
Omit the isolation part of the 2-port cal.
Perform an LO Power Cal.
Set LO power level on External Source (MUST be pre-configured either remotely or using the GUI. See example program.)
Enable and configure phase measurements
The SCPI commands in this example are sent over a COM interface using the SCPIStringParser object. You do NOT need a GPIB connection to run this example. However, some modification is necessary to make the program run on a traditional GPIB Interface. For example, during the power meter portion of this calibration, scpi.Parse will not process a command until the power meter routine has completed. Traditional GPIB would require a serial polling technique to ensure the routine has completed before proceeding.
This VBScript (*.vbs) program can be run as a macro in the VNA. To do this, copy the following code into a text editor file such as Notepad and save it on the VNA hard drive as SMC.vbs. Learn how to setup and run the macro.
|
Dim app Dim scpi ' Create / Get the VNA application. Set app = CreateObject("AgilentPNA835x.Application") Set scpi = app.ScpiStringParser ' Create a Scalar Mixer Forward Measurement 'First, delete all measurements on the channel scpi.Parse "CALC:PAR:DEL:ALL" 'Create a forward scalar mixer measurement and configure it in 'channel 1. The first parameter is a unique 'identifying string (specified by the user) to allow subsequent 'commands to be directed at this specific measurement. scpi.Parse "CALC:CUST:DEF 'My SC21', 'Scalar Mixer/Converter', 'SC21'" 'Setup the new measurement in the active window scpi.Parse "DISP:WIND:TRAC:FEED 'My SC21'" 'Make the new trace the active measurement scpi.Parse "CALC:PAR:SEL 'My SC21'"
'The parameters of the mixer measurement can now be configured. 'This can be done by either using the SENS:MIX commands 'for each of the parameters or by loading a mixer setup file. 'Uncomment the following line to load a mixer setup file. The path name 'for the mixer file may be loaded from other mapped drives. 'scpi.Parse "SENS:MIXer:Load 'c:\users\public\network analyzer\documents/Mixer/MyMixer.mxr'"
' Setup Stimulus ' Points and IFBW are channel settings scpi.Parse "SENS:SWEep:POINts 21" scpi.Parse "SENS:BANDwidth 1e3" ' Mixer settings scpi.Parse "SENS:MIX:INPut:FREQ:MODE SWEPt" scpi.Parse "SENS:MIX:INPut:FREQ:STAR 3.6e9" scpi.Parse "SENS:MIX:INPut:FREQ:STOP 3.9e9" scpi.Parse "SENS:MIX:LO:FREQ:MODE FIXED" scpi.Parse "SENS:MIX:LO:FREQ:FIX 1e9" scpi.Parse "SENS:MIX:LO:POW 10" scpi.Parse "SENS:MIX:OUTP:FREQ:SID LOW" scpi.Parse "SENS:MIX:CALC Output" scpi.Parse "SENS:MIX:APPLY" 'First apply the settings, then set LO Name scpi.Parse "SENS:MIX:LO:NAME 'Port 3'" scpi.Parse "SENS:MIX:APPLY" scpi.Parse "SENS:MIX:SAVE "C:/Program Files/Keysight/Network Analyzer/Documents/Mixer/MyMixer.mxrx"" '--------------Perform A Scalar Mixer Calibration---------------------- 'Specify the connector types and the cal kits for each of the ports. scpi.Parse "SENS:CORR:COLL:GUID:CONN:PORT1:SEL ""APC 3.5 male""" scpi.Parse "SENS:CORR:COLL:GUID:CONN:PORT2:SEL ""APC 3.5 female""" scpi.Parse "SENS:CORR:COLL:GUID:CKIT:PORT1:SEL ""N4691-60004 ECal""" scpi.Parse "SENS:CORR:COLL:GUID:CKIT:PORT2:SEL ""N4691-60004 ECal"""
' Non-factory characterizations are specified as follows: 'scpi.Parse "sens:corr:coll:guid:ckit:port2 'N4691-60004 User 1 ECal'" ' When two or more ECal modules with the same model number are connected ' also specify the serial number as follows: 'scpi.Parse "sens:corr:coll:guid:ckit:port2 'N4691-60004 ECal 01234'" ' When Disk Memory ECal user characterizations are used, ' specify both the User char and the serial number as follows: 'scpi.Parse "sens:corr:coll:guid:ckit:port2 'N4691-60004 MyDskChar ECal 01234'" ' Uncomment the following lines to manually orient ' the ecal port A connected to VNA port 1 'scpi.Parse "SENS:CORR:PREF:ECAL:ORI OFF" 'scpi.Parse "SENS:CORR:PREF:ECAL:PMAP ECAL2 ="A1,B2"
' Specify Mechanical cal kits 'scpi.Parse "sens:corr:coll:guid:ckit:port1 '85033D/E'" 'scpi.Parse "sens:corr:coll:guid:ckit:port2 '85033D/E'"
'Optional settings 'Specify the thru measurement method. 'Always send an INIT command before the Thru command. 'scpi.Parse "SENS:CORR:COLL:GUID:INIT" 'scpi.Parse "SENS:CORR:COLL:GUID:PATH:TMET 1,2,""UNDEFINED THRU""" 'Omit the isolation part of the 2-port cal (default behavior). 'scpi.Parse "SENS:CORR:COLL:GUID:ISOL NONE" ' 'Perform LO Power Cal 'scpi.Parse "SENS:CORR:COLL:GUID:SMC:LO1:PCAL 1" 'Set the LO power level for the cal on an external PSG source. 'scpi.Parse "SENS:CORR:COLL:GUID:PSEN1:POW:LEV 10,’PSG’” ' 'Enable and configure Phase measurements 'scpi.Parse "SENS:MIX:PHAS 1" 'scpi.Parse "SENS:MIX:NORM:POIN 1" 'Using Fixed delay 'scpi.Parse "SENS:CORR:COLL:GUID:SMC:PHAS:METH FIX" 'scpi.Parse "SENS:CORR:COLL:GUID:SMC:PHAS:DEL 12e-9"
'Initialize an SMC guided calibration. scpi.Parse "SENS:CORR:COLL:GUID:INIT" 'Tell the wizard to generate and report the number of steps in this cal. Dim steps Dim desc 'Determine the number of steps required to complete the calibration. steps = scpi.Parse ("SENS:CORR:COLL:GUID:STEP?") For i = 1 To steps 'Display the prompt for each step desc = scpi.Parse ("SENS:CORR:COLL:GUID:DESC? " & CStr(i)) MsgBox (desc) 'Perform the measurement for each step scpi.Parse "SENS:CORR:COLL:GUID:ACQ STAN" & CStr(i) Next 'Finish the cal and save the calset scpi.Parse ("SENS:CORR:COLL:GUID:SAVE ON") Msgbox ("SMC cal saved to CH1_CALREG") |