Basic Measurement Sequence


The following process can be used to setup all analyzer measurements:

Step 1. Set Up Measurements
Reset the analyzer, create a measurement state, and adjust the display.

Step 2. Optimize Measurements
Improve measurement accuracy and throughput using techniques and functions.

Step 3. Perform a Measurement Calibration
Reduce the measurement errors by performing a calibration.

Step 4. Analyze Data
Analyze the measurement results using markers, math operations, and limit tests.

Step 5. Print, Save or Recall Data
Save or print the measurement data.