Dialog Transparency


Most VNA dialogs can be made to appear with various amounts of transparency. This allows you to view the VNA traces through the dialog as you make dialog settings.

How to set Transparency Level

There are three ways to make the transparency level setting:

1. Right-click in any non-control area of a dialog that allows transparency to see the following selections:

2. In tabbed dialogs, cycle through the above transparency settings by pressing multiple times.

3. Launch the Transparency dialog (below) from the Preferences dialog.

 

This setting is not programmable

 

Dialog Transparency dialog box help  

Note: This single Transparency setting applies to ALL supported VNA dialogs.

  • Opaque (NOT Transparent) - Default setting

  • 8% Transparency

  • 25% Transparency

  • 50% Transparency

Double-click changes transparency - When checked, cycle through the above transparency settings by double-clicking in any non-control area of a dialog that allows transparency.

Notes

  • The transparency setting is stored as a VNA Preference.

  • The setting survives a VNA Shutdown and Preset.

  • It is NOT saved and recalled with instrument state.