|
Switch Path dialog box help |
|
Switch PathBy Test Port Number – Set displaying port number in the “Test Port” combo-Boxes By Test Port Label – Set displaying port label in the “Test Port” Combo-boxes VNA Port - Shows the VNA port number Test Port - Select test port by number or label from the pulldown list. Note: The path will not be switched until user click the “Apply” button, in order to save the switch matrix service lifetime. Test Port LabelTest Port Number - Shows switch matrix test port numbers Test Port Label - User can edit port labels. They are per-channel settings, different channels can have different port labels. Labels will be saved in state file. De-embeddingEnable De-embedding Switch Paths - Sets de-embedding switch matrix state on/off. By default, it is checked. Apply the Cal Set stimulus to the channel - Check to apply the Cal Set stimulus values to the channel. Tier 1 Cal Set - Selects Tier 1 Cal Set.
Channel - Default channel is E-TDR. User can select another Standard channel if exists. Apply - Apply settings:
OK - Apply settings and close dialog.
|