The Option S96041B Impedance Measurement application measures the impedance parameter up to 10 GHz with E5080B.
The following calibration kit and test fixture are required to make a measurement.
85052DH02 Economy Mechanical Calibration Kit (85052DH02 is different from 85052D. The calibration data file for each unit is provided.)
16198A Bottom Electrode SMD Test Fixture (Option 010 only)
Note: E5080B over 20 GHz models are not supported.
This section shows you the required preparation before you make an measurement.
Prepare the following items
85052DH02
Open (female), Short (female), Load (female)
Calibration data file: This file is provided by USB memory furnished with the product.
16198A Option 010 (See the 16198A user's guide in https://www.keysight.com/manuals/16198a for details)
Fixture with a contact board and weight.
Adapter Box
Semi-rigid cable between Adapter Box and VNA
Short bar
Calibration Data (See the next step)
Torque wrenches
Each unit of 16198A Option 010 is calibrated at the factory and its calibration data is provided though Keysight support website.
Visit https://support.keysight.com/. Click Calibration Certificate in SERVICES.
Enter 16198A as the product number and your serial number. The serial number label is placed on the right side of fixture main unit. The serial number is 10 digit number beginning with MY or SG.(Do not use the number beginning with 1B)
Select SERVICE STATUS / CAL DOCS tab.
Confirm the certificate number
starts with FACT-KEYS-1Bxxxxxxxxx. The 10 digit number beginning
with 1B is the manufacturing ID. Confirm if this number is matched
with the number labeled on the left side of fixture main unit.

If the manufacturing ID number
is NOT matched with the number labeled on the left side of fixure
main unit, visit Support
top page again and enter manufacturing ID number instead of the
serial number.
Note: If your unit is repaired, the serial number is kept but the
manufacturing number is changed if the calibration data is updated.
Click the Characterization Data under Service Documents.
The calibration data is stored as ZIP file. Download and extract it. The file extension is ".dat".
Move the .dat file into E5080B.
Place the Adapter box in front of the E5080B and connect it with the E5080B through the Semi-Rigid cable. The tightening torque used is 0.9 Nm for 3.5 mm and 1.36 Nm for Type N
The wear check allows you to obtain an idea about the deterioration of the fixture in order to ensure that the desired measurement accuracy is obtained.
Refer to the 16198A Users Guide for the test limit.
Preset
Click Meas > S-Param > Sxx (S22, S33 or S44) if the adapter box is connected with other than port 1.
Click Freq > Main > Start, Stop and set start and stop frequencies at 1 GHz and 3 GHz respectively.
Click Power > Main > Power Level and set the power level at -16 dBm.
Click Cal > Other Cals > Basic Cal.
Connector: 3.5 mm
Cal Kit: your 85052DH02 calkit.
VNA Port: Check only the port where the adapter box is connected.
DUT: Female
Cal Type:OSL
Click Next, then execute Open/Short/Load calibrations.
Click Finish.
Click Math > Analysis > Conversions > Y-Reflect.
Click Format > Format 2 > Real.
Take measurements of the data for the open state.
Click Marker > Marker 1 and 2, then move the markers at 1 GHz and 3 GHz.
Compare the result with the limit.
Setup and Calibration is the same as the open state
Click Math > Analysis > Conversions > Z-Reflect.
Click Format > Format 2 > Real.
Set the 200 to 300 g weight.
Place a short bar at the right position on the contact board.
Set the fixture in the short state
Make sure if the pusher pushes the short bar properly
Take measurements of the data for short bar.
Click Marker > Marker 1 and 2, then move the markers at 1 GHz and 3 GHz.
Compare the result with the limit.