MWA Operational Requirements


Requirements for operating the MWA software are as follows:

A PC for running the front-end application

The E5080A Network Analyzer

Note: The MWA operates only when the number of channels is three or more (four or more for the VNA settings).

Multiport Test Set 

If you wish to make multiport measurements, the following multiport test set are supported by the MWA.

Note: Up to two multiport test set can be used.

ECal Module

When using the ECal module with calibration wizard in the back-end application of the MWA, the 4-port ECal module supported by the VNA is required. Refer to ECal for supported ECal modules by the VNA.