Other topics about Measurement Wizard Assistant
The MWA consists of a front-end application, which creates spec sheets on the PC, and a back-end application, which makes measurements with the VNA. Each of the installation procedures is described below.
Follow the procedure below to install the front-end application program of the MWA on the PC:
Download MWA software evaluation version from http://www.keysight.com/find/mwa/.
Extract the MWA software package.
Copy mwa_xxxx.xlsm (x in mwa_xxxx.xlsm means revision number. e.g.: mwa_0106.xlsm) to an appropriate folder on the PC.
When your VNA is equipped with option S96790A or 790, the MWA back-end application (mwa.exe) has already been installed on the C:\Program Files (x86)\agilent\network analyzer\applications\mwa at the factory shipment.