Starting and Exiting Modulation Distortion

In this topic:

Starting Modulation Distortion Application

How to start Modulation Distortion

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. On the VNA, press Meas > S-Param > Meas Class....

  2. Select Modulation Distortion, then click OK.

  3. In the Confirm Measurement Class Change dialog, click OK to proceed or Cancel to exit.

  4. The Modulation Distortion application is displayed (shown below).

  1. Click Instrument.

  2. Select Meas Class....

  3. Select Modulation Distortion, then click OK.

  4. In the Confirm Measurement Class Change dialog, click OK to proceed or Cancel to exit.

  5. The Modulation Distortion application is displayed (shown below).

Programming Commands

 

Exiting Modulation Distortion Application

  1. Select a different Measurement Class for the currently active channel.