Frequency Offset measurements require the VNA source to tune to a different frequency than the VNA receiver.
This capability is offered as S96082A or E5080A-009. E5080A-009 and S96082A are identical in functionality.
To view the options that are installed on your VNA, click Help then About Network Analyzer