SENSe:TEMPerature? <char>,<mod>

Applicable Models: M937xA,M98xxA, P93xxA/B, P50xxA/B, E5080B, E5081A

(Read-only) Returns the temperature on the Receiver microcircuit.

  • To read temperature from the SFP, press System, then Service, then Utilities, then Receiver Temperature.

  • The temperature reading is updated with every sweep.

Parameters

 

<char>

Choose from CELSius or FAHRenheit

<mod>

Module number for PXI. If unspecified, value is set to 1. Learn how to determine module number.

Examples

SENS:TEMP? CELS
sense:temperature? fahrenheit,2

Return Type

Numeric

Default

Not Applicable