This example program creates a Differential I/Q measurement setup.
This VBScript program can be run as a macro in the VNA. To do this, copy the code into a text editor file such as Notepad and save on the VNA hard drive as DIQ.vbs. Learn how to setup and run the macro.
See the Differential I/Q commands.
See Other SCPI Example Programs
|
' This section gets the VNA application ' starts the scpi parser, and presets the VNA Set app = CreateObject("AgilentPNA835x.Application") Set scpi= app.ScpiStringParser scpi.Parse "SYST:FPR" scpi.Parse "CALC:CUST:DEF 'mytrace','Differential I/Q','IPwrF1'" scpi.Parse "DISP:WIND ON" scpi.Parse "DISP:WIND:TRAC:FEED 'mytrace'" scpi.Parse "SENS:DIQ:FREQ:RANG:ADD" scpi.Parse "SENS:DIQ:FREQ:RANG1:STARt 1e9" scpi.Parse "SENS:DIQ:FREQ:RANG1:STOP 2e9" scpi.Parse "SENS:DIQ:FREQ:RANG2:COUP:STATe ON" scpi.Parse "SENS:DIQ:FREQ:RANG2:COUP:ID 1" scpi.Parse "SENS:DIQ:FREQ:RANG2:COUP:MULT 2" scpi.Parse "SENS:DIQ:PORT1:RANG 1" scpi.Parse "SENS:DIQ:PORT1:STATe ON" scpi.Parse "SENS:DIQ:PORT1:MATC:STATe ON" scpi.Parse "SENS:DIQ:PORT1:MATC:RANGe 'F1'" scpi.Parse "SENS:DIQ:PORT1:MATC:TREC 'b3'" scpi.Parse "SENS:DIQ:PORT1:MATC:RREC 'a3'" scpi.Parse "SENS:DIQ:PORT1:POW:SWE:STATe OFF" scpi.Parse "SENS:DIQ:PORT1:POW:STARt -5" scpi.Parse "SENS:DIQ:PORT:POW:ATT 5" scpi.Parse "SENS:DIQ:PORT:POW:ATT:AUTO ON" |