This Python example program polls for the completion of a sweep.
|
import time import pyvisa as visa
def write_with_stb_polling(session,command,timeout): # Enable operation complete status register session.write("*ESE 1")
# Clear the existing status state session.query("*ESR?")
# Send asynchronous command session.write(command)
# *OPC indicates that we want to be notified when the asyn command is completed # Note that we are NOT using the query form, so this does not block session.write("*OPC")
# Check if the asyn operation has completed by checking bit 5 (32) isDone = session.read_stb() & 32 end_time = time.time() + timeout while (not isDone and time.time() < end_time): time.sleep(0.1) # sleep for 100 ms to avoid working the CPU isDone = session.read_stb() & 32
# If still not done, then it is because the timeout was hit # Report it as an exception if (not isDone): raise Exception(f"Timeout exceeded ({timeout}s) with {command}")
# Change this variable to the address of your instrument # or leave this alone when using the simulator VISA_ADDRESS = 'TCPIP0::localhost::inst0::INSTR'
# Create a connection (session) to the instrument resourceManager = visa.ResourceManager() session = resourceManager.open_resource(VISA_ADDRESS)
# Command to preset the instrument and deletes the default trace, measurement, and window session.write("SYST:FPR")
# Create and turn on window 1 session.write("DISP:WIND1:STAT ON")
# Create the measurement session.write("CALC1:MEAS1:DEF 'S11'")
# Displays measurement 1 in window 1 and assigns the next available trace number to the measurement session.write("DISP:MEAS1:FEED 1")
# Set the channel into hold mode session.write("SENS:SWE:MODE HOLD")
# Set sweep time to 2 seconds to simulate a slow sweep session.write("SENS:SWE:TIME 2")
print("Start Sweep") timeoutForCommand = 10 # 10 seconds timeout write_with_stb_polling(session,"SENS:SWE:MODE SING",timeoutForCommand) print("Stop Sweep")
|