Software Support

Each software license includes free software updates and support for the specific instrument application for the duration of your support subscription. A perpetual license term includes software updates and support for the first year, after which support can be renewed annually for a fee. A subscription-based license term includes software updates and support through the term of the license.

In this topic:

List of Gated Licensed Features

The following table is a list of all features that are "gated" (or tied) to specific software licenses. Software licenses must be active to use "gated" features. Click on a gated feature link below to access a description. The Licensed Features dialog displays the licensed features in your instrument.

 

Model

Description

Licensed Feature (Release Date)

S9x007B

Automatic Fixture Removal

AFR Config and 2X Thru for N Port  (2021.0506)

Cal Update (refer to Cal Update and AFR topics) (2022.0101)

S9x010B

Time Domain

TD Transform Window (2021.1101)

S9x011B

Enhanced time domain analysis with TDR

L8990M Switch Matrix (2022.0211)

TD Transform Window (2021.1101)

S9x015B

Real-time S-Parameter and Power Measurement Uncertainty

None

S9x024B

Basic Pulsed-RF Measurements, Lite

Plot Pulse Dialog (2023.1128)

S9x025B

Basic Pulsed-RF Measurements

Plot Pulse Dialog (2023.1128)

S9x027B

Mechanical noise tuner control

Focus Microwaves Tuner Support (2023.0601)

S9x029B

Noise Figure Measurements with Vector Correction

Mixer CSV Format (2021.0820)

Support for U1832X and U1833X Noise Sources (2021.0903)

Macro Control for NF measurement path switching (2022.0910)

Multi-sensor Power Calibration for SMC/GCX (2022.0910)

External Noise Amplifier

S9x070B

Modulation Distortion

Mixer CSV Format (2021.0820)

Create Digital Modulation (2022.0601)

Multi-sensor Power Calibration for SMC/GCX (2022.0910)

Multi-sensor Power Calibration for SMC/GCX (2022.0910)

Digital Pre-Distortion (DPD) and Single Port EVM Analysis (2022.0601)

S9x082B

Scalar Mixer Converter (SMC) measurements

Mixer CSV Format (2021.0820)

Multi-sensor Power Calibration for SMC/GCX (2022.0910)

S9x083B

Vector & Scalar Mixer/Converter Measurements

Mixer CSV Format (2021.0820)

Multi-sensor Power Calibration for SMC/GCX (2022.0910)

S9x084B

Embedded LO Capability

Mixer CSV Format (2021.0820)

Multi-sensor Power Calibration for SMC/GCX (2022.0910)

S9x086B

Gain-Compression Measurements

Gain Compression Phase

Mixer CSV Format (2021.0820)

Multi-sensor Power Calibration for SMC/GCX (2022.0910)

Parallel Gain Compression Measurement for Amplifiers (2024.0101)

S9x087B

Swept IMD for Amplifiers

IMD: Multiple Receiver Configurations (2022.0601)

Mixer CSV Format (2021.0820)

Multi-sensor Power Calibration for SMC/GCX (2022.0910)

S9x088B

Source Phase Control

None

S9x089B

Differential and I/Q device measurements

Mixer CSV Format (2021.0820)

Multi-sensor Power Calibration for SMC/GCX (2022.0910)

S9x090B

Spectrum Analysis

Mixer CSV Format (2021.0820)

Create Digital Modulation (2022.0601)

Multi-sensor Power Calibration for SMC/GCX (2022.0910)

S9x460B

True-Mode Stimulus

None

S9x551B

Multiple Instruments/modules measurements

None

Note: The M983xA requires the valid subscription.

S9x552B

Multiport calibration assistant / Multiport ECal for PXI Switches

None

S9x553B

Multiport calibrated measurements with switch instruments

None

License Types

Node-locked (Fixed)

This type of license is locked to a specific host instrument or PC, and only allows use of the product on this host.

Use node-locked licenses when your product only needs to be used with a single instrument or PC. It provides the most cost-effective alternative for single-use situations.

 

Transportable

This type of license is provisionally locked to a specific host instrument or PC, and only allows use of the product on this host, but it can be unlocked from one host and then locked to another host. You can do this using PathWave License ManagerKeysight License Manager 5, or Keysight Software Manager.

Use transportable licenses when your product periodically needs to be used on a different instrument or PC. The transport process enables product use to be shifted between physically adjacent instruments or PCs, and also between geographically distributed instruments or PCs.

 

USB Portable

This type of license is locked to a USB key (sold separately), and can be physically moved from one host instrument or PC to another with that USB key. When connected to a host, the USB key enables the use of the product on that host. This enables multiple users who are physically adjacent to share licenses without being connected to a network.

Use USB portable licenses when your product needs to be shared frequently among different instruments or PCs and multiple users, and the instruments or PCs may not always be connected to a common network.

USB portable licenses require installing an additional software driver. See Keysight Licensing USB Driver.

 

Floating (Network)

This type of license is locked to a license server, a host PC that manage pools of licenses. The licenses can be used by multiple users on multiple instruments or PCs; the license server ensures that each purchased license count is used by only one user at a time. This enables geographically-distributed users to share licenses across a common network. 

Use floating licenses when your product needs to be shared frequently among different instruments or PCs and among multiple users, and you have a common network that can interconnect all the instruments and PCs with the license server.

License Terms

Perpetual (Permanent)

This term of license usage allows you to use the product indefinitely.

Perpetual licenses include software updates and support for the first year. Support may be renewed annually for a fee after that.

Use perpetual licenses when you will need to use the product for an extended period of time (e.g. many years) and you may not need updates and support after the first year.

 

Subscription (Expiring)

This term of license usage allows you to use the product for a specific limited time.

Subscription licenses include software updates and support through the term of the license.

Software Support Dialogs

There are three dialogs that provide support information:

Access Software Support

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Press System > Help > Tech Support.

  2. Select My Software Support... or My Support ID....

  1. Click Help.

  2. Select Tech Support.

  3. Select My Software Support... or My Support ID....

My Software Support

This dialog displays software-specific support information.

Model Number - Displays the model number of the feature.

Description - Displays a description of the feature.

Support Expiration - Displays the support expiration date.

License Expiration - Displays the license type.

Contact Keysight... button - Opens the dialog showing contact information:

My Support ID

This dialog displays your support IDs used to register for software updates, services, and technical support. The support ID is typically the same as the host ID used to serve licenses. Your product configuration may have more than one support ID, each comprised of multiple fields of information.

Model Number - Displays the model number of the feature.

Description - Displays a description of the feature.

Support ID - Displays your support ID, which is typically the same as the host ID.

Copy icon - Copy the corresponding ID information to the clipboard.

Copy All to Clipboard... button - Copies all the contents of this dialog to the clipboard.

Licensed Features

Programming Commands

This dialog displays a list of new features in the VNA firmware and corresponding license.

On start-up, the following dialog appears if the Show Disabled Features at Startup is checked and at least one feature has an expired support contract.

In the normal case, all licenses are shown.

 

Feature Name - Displays the name of the measurement feature.

Feature Release - Displays the license model firmware release date.

Model Number Linked to Feature - Displays the licenses that can enable the feature. Each license is on its own line with the expiration data. This information can also be found in the Keysight License Manager. Support contract information is NOT in the Keysight License Manager.

Enabled - Indicates whether the feature is enabled or not. When the Feature Release date is newer than the date in Model Number Linked to Feature, the feature is disabled. Purchase the subscription for the software to enable the feature.

Help - Link to information about the feature.

Show Disabled Features at Startup - When enabled, will display the Disabled Licensed Features dialog at startup. If unchecked and default preferences are restored, the Show Disabled Features at Startup will be checked.