Source Power Alignment

This function is available on E5080B and E5081A.

The Source Power Alignment is a tool to improve the power level linearity. The analyzer has a source step attenuator (6 dB step from 0 dB to 90 dB [Up tp 20 GHz]  or 5 dB step from 0 to 90 dB [above 20 GHz] attenuation ) for the power output level control. The power linearity may become worse at the point where the step attenuator setting is changed although it is within the specification. After executing this source power alignment, the linearity will be improved.

How to execute the source power alignment

Use one of the following methods

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Press Macro > Macro1 > Src Power Alignment

  1. Click Utility > Macro  > Src Power Alignment [sourcepoweral...]

Note: System > System Setup > Remote Interface > Hislip must be enabled before the execution. The hislip address must be set at 0.

Note: When the macro button is not available, execute “C:\\Program Files\Keysight\Network Analyzer\Service\sourcepoweralignement.exe”

Note: When you want to use a different hislip address, execute “C:\\Program Files\Keysight\Network Analyzer\Service\sourcepoweralignement.exe” / address TCPIP::localhost::hislip2::INSTR, for example

Source Power Alignment dialog box help

Alignment Power Range: select the power range you will use. Wider range will take longer time for execution.

If you do not measure at lower level, selecting -40 dBm or -50 dBm to +20 dBm (E5080B, E5081A ports 3 and 4) / +30 dBm (E5081A ports 1 and 2) reduces the execution time.

Target Module Selection: select the required module

Alignment Status: show the current status.

Alignment On enables/disables the alignment data you took.

VISA address: display the VISA address for hislip.

Take Alignment Sweep: Start the source power alignment. The measurement display would not be updated. A progress bar will show you the progress of task. The firmware restart is required at the end of task.

 

Limitations for Ports 1 and 2 on E5081A

Frequency Range

Minimum Power Limit

Min frequency to 10 MHz

N/A (Source alignment is not applied)

10 MHz to 100 MHz

- 40 dBm

100 MHz to max frequency

User specified power range lower level (-60 , -50 or -40 dBm)