Last Updated: August 29, 2007
The Performance Tests in the Calibration Software are required for:
As part of a normal test equipment audit the performance of the test set should be verified using the N7805A Wireless Communications Test Set Calibration Software. This should be done before any adjustments are made to determine if the test set is functioning correctly.
When the test set has been repaired or after a hardware upgrade it is adjusted using the Adjustment Software included with the N7805A Wireless Communications Test Set Calibration Software. The Adjustment Software calibrates the test set to meet factory specifications.
After adjusting the test set it should be verified using the Performance Tests in the N7805A Wireless Communications Test Set Calibration Software.