Analog Out

Output Enabled  Turns on or off the analog output signal

Voltage Level  Sets the output voltage level

Range  Selects the current range of output from 50 m or 500 mA

Pulse Modulate  Enable the pulse modulation for Analog Out.  Analog Outs 1 an 2 are synchronized with a TTL signal into SMB sync 4 port. At default, it is positive logic. When the TTL signal is high, the analog out is outputted. Its polarity can be changed by IKtM9341AnalogIOOutputPulseModulation.Polarity.  When SMB sync 4 port is open, TTL signal should be high because it is pulled up.

Over-current Protection  Shows the status of signal output, Output On or Output Off. Note that when the protection turns off the output, the "DC Source" dialog the state of the analog output may still indicate that it is "on" because this state is independent of the protection.

Reset Protection  Resets the over-current protection for all channels

Refresh Protection Status  Updates the protection status at the latest

Analog Out 1/2 Output Current Measure  executes the analog output current monitor measurement and show the result for analog output current level.

Measurement Time   Specifies the measurement time. This can calculated by (Number of Samples) x 20 nsec. This is the same entry in Analog In Tab.

Number of Samples  Specifies number of ADC samples for one point. One ADC sample takes 20 nsec. Increasing this number improves the stability of DC measurement. This is the same entry in Analog In Tab.

Calibrate Analog Out Level  Executes the analog out calibration. No setup is required for calibration. Validation of calibration: 1 hour and ±3 cº from previous  calibration.  Over-current protection status should be "Output On" for this calibration.