5G NR
Generates a waveform based on your application's (e.g. 5G NR) current configuration. Also use this function to check for waveform errors before downloading or exporting the waveform.
When generating a waveform, the following parameters are verified. If any conflicts are found, the waveform generation will be canceled.
Channel valid checking. If any channel is invalid, error + 690 "5GNR error; Generation failed because $Channel is not valid" will be shown.
Channel conflict checking. If any two channels conflict, error + 690 "5GNR error; Generation failed because $Channel has conflicts" will be shown.
Payload Data checking. If enabled payload data is invalid , error will be shown. Please refer to Payload section for more detailed information.
|
GUI Location |
Apps > 5G NR > Generate |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:GENerate |
|
SCPI Example |
RAD:NR5G:WAV:GEN |
|
Notes |
It is an overlap SCPI |
|
State Saved |
No |
|
Initial S/W Revision |
A.01.00 |
|
Modified S/W Revision |
A.09.00 |