Connectors

Connector routing is supported only on the M9484C. Connector routing is used to associate the physical connectors to features of signal generation.

Trigger

Events

STrig (Sync Trigger)

Trigger Input

Trigger Output

Global Trigger

STrig In

Slope

Delay

Hold Off

Threshold

Function

Polarity

Delay

Pulse Width

Source

Routing

Output Polarity

Output Delay

Input Delay

Input Slope

Input Threshold

Auxiliary LO

LF Out

LO 1

LO 2

State

Amplitude

DC Offset

Source

Frequency

Frequency Increment

Phase Offset

Shape

Shape Ramp Polarity

Duty Cycle

Function 1

Trigger

For the M9484C, Trigger Connectors can be used for routing as input or output. The available connectors are based on the instrument’s channels and options:

Connectors Trig A, Trig B, Trig C output bandwidth is limited to 100 MHz; when they are set for output, 3.3 V is the high voltage

Connectors AIO 1 through AIO 12 the input bandwidth is limited to 1 MHz

Via SCPI the connectors are referenced by a number; 1 to the maximum number of connectors. A SCPI command can be used to provide the connector label for the corresponding number.

SCPI Command

:ROUTe[:CONNectors][:RF<channel>]:TRIG<connector>:LABel?

SCPI Example

ROUT:CONN:RF1:TRIG1:LABel?

Notes

The query result will be the labels on the front or rear panel of the instrument. The return value is a string that may contain whitespace characters; for example “Trig A”.

For M9484C:

For Channel 1 without Option AN1, and channels 2, 3, 4:

1 = “Trig 1”

2 = “Trig 2”

3 = “Trig 3”

For Channel 1 with Option AN1:

1 = “Trig 1”

4 = “Trig A”

5 = “Trig B”

6 = “Trig C”

7 = “AIO 1”

8 = “AIO 2”

…

18 = “AIO 12”

 

It is recommended that you do not query the connector labels for the specific options of the instrument. Attempting to query the label of a connector will raise error -200,”Execution Error”. See Query Options per Channel.

Dependencies

RF1:TRIG1|4|5|6|7|8|9|10|11|12|13|14|15|16|17|18 are available connectors when Option AN1 is present.

RF1 available connectors without Option AN1 are TRIG[1]|2|3.

RF2|3|4 available connectors are TRIG[1]|2|3.

Attempting to send TRIG<number> for connectors that don’t exist on the instrument will generate an Execution Error

State Saved

N/A

Initial S/W Revision

A.09.00

Trigger Input

Supported only on the M9484C.

ClosedView image.

The physical trigger connectors can be used as inputs or outputs. As trigger inputs their operation is applicable when the Configuration Group for the channel is Independent. When the Configuration Group is not Independent see Global Trigger. For instruments with Option 8SG the trigger input can be directed to each Signal.

When a trigger connector is used as an input, the following settings can be configured.

Slope

For the M9484C, sets the polarity of the signal input at the channel’s trigger connector.

SCPI Command

:ROUTe[:CONNectors][:RF<channel>]:TRIG<connector>:INPut:SLOPe POSitive|NEGative

:ROUTe[:CONNectors][:RF<channel>]:TRIG<connector>:INPut:SLOPe?

SCPI Example

ROUT:CONN:RF1:TRIG1:INP:SLOP NEG

ROUT:CONN:RF1:TRIG1:INP:SLOP?

Notes

Attempting to send TRIG<number> for connectors that don’t exist on the instrument will generate an Execution Error.

Preset

POSitive

Range

Negative | Positive

State Saved

Yes

Initial S/W Revision

A.09.00

Delay

For the M9484C, sets the input delay of a trigger connector.

SCPI Command

:ROUTe[:CONNectors][:RF<channel>]:TRIG<connector>:INPut:DELay timeSec

:ROUTe[:CONNectors][:RF<channel>]:TRIG<connector>:INPut:DELay?

SCPI Example

ROUT:CONN:RF1:TRIG1:INP:DEL 5 us

ROUT:CONN:RF1:TRIG1:INP:DEL?

Notes

Attempting to send TRIG<number> for connectors that don’t exist on the instrument will generate an Execution Error.

Preset

0 s

State Saved

Yes

Min

0 s

Max

6.825 us

Resolution

1.666… ns

Initial S/W Revision

A.09.00

Hold Off

For the M9484C, sets the minimum time after an edge trigger before the system can perceive the next edge trigger. A trigger edge during this time period will be lost. This feature helps avoid double-triggering with a noisy or “bouncing” input signal.

SCPI Command

:ROUTe[:CONNectors][:RF<channel>]:TRIG<connector>:INPut:HOLDoff timeSec

:ROUTe[:CONNectors][:RF<channel>]:TRIG<connector>:INPut:HOLDoff?

SCPI Example

ROUT:CONN:RF1:TRIG1:INP:HOLD 2 s

ROUT:CONN:RF1:TRIG1:INP:HOLD?

Notes

Attempting to send TRIG<number> for connectors that don’t exist on the instrument will generate an Execution Error.

Preset

10 ns

State Saved

Yes

Min

10 ns

Max

3.5 s

Resolution

1.666… ns

Initial S/W Revision

A.09.00

Threshold

For the M9484C, sets the level above/below which the input signal is considered high vs low. Some connectors have fixed threshold levels.

For instruments that have Trig2 and Trig3, the threshold is fixed at 1.8 V CMOS.

For instruments that have AIO1 through AIO12, the threshold is fixed at 3.3 V CMOS.

SCPI Command

:ROUTe[:CONNectors][:RF<channel>]:TRIG<connector>:INPut:THReshold <voltage>

:ROUTe[:CONNectors][:RF<channel>]:TRIG<connector>:INPut:THReshold?

SCPI Example

ROUT:CONN:RF1:TRIG:INP:THR 1.5 V

ROUT:CONN:RF1:TRIG:INP:THR?

Notes

Attempting to send TRIG<number> for connectors that don’t exist on the instrument will generate an Execution Error.

Attempting to change value of TRIG<number> for connectors that have fixed values will generate an error.

Preset

1 V

State Saved

Yes

Min

Trig1: 0.5 V

Trig2, Trig3: 1.8 V (Fixed)

Trig4, Trig5, Trig6: 0.5 V

Trig7 – Trig 18: 3.3 V (Fixed)

Max

Trig1: 2.5 V

Trig2, Trig3: 1.8 V (Fixed)

Trig4, Trig5, Trig6: 5 V

Trig7 – Trig 18: 3.3 V (Fixed)

Resolution

Trig1: 100 mV

Trig4, Trig5, Trig6: 9.765625 mV

State Saved

Yes

Initial S/W Revision

A.09.00

Trigger Output

Supported only on the M9484C.

ClosedView image.

The physical trigger connectors can be used as inputs or outputs. When a trigger connector is used as an output, the following settings can be configured.

Function

For the M9484C, routes a signal to a trigger connector for output.

Output routing options:

SCPI Command

:ROUTe[:CONNectors][:RF<channel>]:TRIG<connector>:OUTPut NONE|SETTled|EVENt<1-3>

:ROUTe[:CONNectors][:RF<channel>]:TRIG<connector>:OUTPut?

SCPI Example

ROUT:CONN:RF1:TRIG1:OUTP EVEN1

ROUT:CONN:RF1:TRIG1:OUTP?

Notes

Attempting to send TRIG<number> for connectors that don’t exist on the instrument will generate an Execution Error

Couplings

If the specified connector was being used as an input by any feature, then the trigger input type for those feature(s) is set to Trigger Key and a Settings Conflict error message is generated.

Preset

NONE

Range

None | Source Settled | Event1 | Event2 | Event3

State Saved

Yes

Initial S/W Revision

A.09.00

Polarity

For the M9484C, sets the polarity of the signal output at the trigger connector.

SCPI Command

:ROUTe[:CONNectors][:RF<channel>]:TRIG<connector>:OUTPut:POLarity POSitive|NEGative

:ROUTe[:CONNectors][:RF<channel>]:TRIG<connector>:OUTPut:POLarity?

SCPI Example

ROUT:CONN:RF1:TRIG1:OUTP:POL POS

ROUT:CONN:RF1:TRIG1:OUTP:POL?

Notes

Attempting to send TRIG<number> for connectors that don’t exist on the instrument will generate an Execution Error.

Preset

POSitive

Range

Negative | Positive

State Saved

Yes

Initial S/W Revision

A.09.00

Delay

For the M9484C, sets the output delay of a trigger connector, its value is independent of any other delays applied to the signal being output.

SCPI Command

:ROUTe[:CONNectors][:RF<channel>]:TRIG<connector>:OUTPut:DELay timeSec

:ROUTe[:CONNectors][:RF<channel>]:TRIG<connector>:OUTPut:DELay?

SCPI Example

ROUT:CONN:RF1:TRIG1:OUTP:DEL 5 us

ROUT:CONN:RF1:TRIG1:OUTP:DEL?

Notes

Attempting to send TRIG<number> for connectors that don’t exist on the instrument will generate an Execution Error.

Preset

0 s

State Saved

Yes

Min

0 s

Max

6.825 us

Resolution

1.666… ns

Initial S/W Revision

A.09.00

Pulse Width

For the M9484C, sets the minimum duration of the trigger output level, helping make sure that outputs are wide enough in time to trigger external equipment. Note: If the trigger event transitions to inactive and back to active during the initial width, that event is lost and does not extend the width.

SCPI Command

:ROUTe[:CONNectors][:RF<channel>]:TRIG<connector>:OUTPut:WIDTh timeSec

:ROUTe[:CONNectors][:RF<channel>]:TRIG<connector>:OUTPut:WIDTh?

SCPI Example

ROUT:CONN:RF1:TRIG1:OUTP:WIDT 5 s

ROUT:CONN:RF1:TRIG1:OUTP:WIDT?

Notes

Attempting to send TRIG<number> for connectors that don’t exist on the instrument will generate an Execution Error.

Preset

50 ns

State Saved

Yes

Min

10 ns

Max

7 s

Resolution

1.666… ns to double precision

Initial S/W Revision

A.09.00

Events

Supported only on the M9484C.

ClosedView image.

These three, output-only connectors have precise timing (at 3 GHz) for markers on baseband signals. The maximum rate of change is 600 MHz. If an Event output is configured to change too quickly, the output will only change on 600 MHz boundaries, regaining the proper level and precise timing wherever the rate of change is 600 MHz or less.

Routing

For the M9484C, Event connector routing can output markers from one or more signals, given the following criteria:

  1. For each connector, only one marker can be selected from each signal.

  2. Only per-signal marker selections for a connector can be ORed together. Note: If any are asserted, the output is asserted.

  3. Per-signal marker selections cannot be combined with None or the single uniform Marker for all signals.

Event routing options:

SCPI Command

:ROUTe[:CONNectors][:RF<channel>]:EVENt{1:3} NONE|M1|M2|M3|M4|signalMarkerSource1[,signalMarkerSource2,…[,signalMarkerSource<signalCount>]]

:ROUTe[:CONNectors][:RF<channel>]:EVENt{1:3}?

signalMarkerSource<n>=S1M1|S2M1|…|S8M4

SCPI Example

ROUT:CONN:RF1:EVEN1 S1M2

ROUT:CONN:RF1:EVEN1 S1M1,S2M1,S3M2

ROUT:CONN:RF1:EVEN1?

Notes

This SCPI command is not additive; sending it clears the Event’s previous output routing and sets them only to the options contained in the command. Additive tweaking of the Event’s output routing can be done manually on the front panel display.

Querying the event will return the sorted order of the list of signalMarkerSource items selected.

Preset

Event1: S1M1

Event2: S1M2

Event3: S1M3

Range

None | Marker1 | Marker2 | Marker3 | Marker4 | Signal Marker Source<n>

State Saved

Yes

Initial S/W Revision

A.09.00

Output Polarity

For the M9484C, sets the polarity of the signal output at the channel’s event connector.

SCPI Command

:ROUTe[:CONNectors][:RF<channel>]:EVENt{1:3}:POLarity POSitive|NEGative

:ROUTe[:CONNectors][:RF<channel>]:EVENt{1:3}:POLarity?

SCPI Example

ROUT:CONN:RF1:EVEN1:POL NEG

ROUT:CONN:RF1:EVEN1:POL?

Preset

POSitive

Range

Negative | Positive

State Saved

Yes

Initial S/W Revision

A.09.00

Output Delay

For the M9484C, sets the output delay at the channel’s event connector, its value is independent of any other delays applied to the signal being output.

SCPI Command

:ROUTe[:CONNectors][:RF<channel>]:EVENt{1:3}:DELay timeSec

:ROUTe[:CONNectors][:RF<channel>]:EVENt{1:3}:DELay?

SCPI Example

ROUT:CONN:RF1:EVEN1:DEL 50 ns

ROUT:CONN:RF1:EVEN1:DEL?

Preset

0 s

State Saved

Yes

Min

0 s

Max

32.3958333333333 ns

Resolution

52.0833… ps

Initial S/W Revision

A.09.00

Modified S/W Revision

A.10.00 Max value changed to 32.3958333333333 ns

Auxiliary LO

For M9484C with Option AL2.

ClosedView image.

For M9484C with option AL2. The instrument contains two connectors labeled LO1 and LO2 for providing an Auxiliary Local Oscillator output. Each connector can be off, or provide a CW frequency of 2.4 GHz, 4.8 GHz, 9.6 GHz, or 19.2 GHz. If you are not using the output, place the setting in off to minimize emissions.

When using V3080A, the Auxiliary LO connector(s) are used for interfacing with V3080A. With a V3080A connected the auxiliary LO port is set to 9.6 GHz and not changeable. When one V3080A is connected to the instrument the LO1 will be used, if a second V3080A is connected LO2 will be used.

SCPI Command

:ROUTe[:CONNectors]:ALOScillator[1]|2 OFF|F2_4|F4_8|F9_6|F19_2

:ROUTe[:CONNectors]:ALOScillator[1]|2?

SCPI Example

ROUT:ALOS2 F9_6

Notes

If Option AL2 is not present, attempting to change ALOS raises error 703,"Feature not supported; Auxiliary LO unavailable on this instrument"

Couplings

When one or more V3080A are in use the Auxiliary LO is set to 9.6 GHz, and not changeable. For the first V3080A detected ALOS1 will be set to 9.6 GHz, when a second V3080A is detected ALOS2 will be set to 9.6 GHz.

Attempting to change the Auxiliary LO with V3080A connected will raise the error "-221, Settings conflict; cannot change Auxiliary LO with V3080A connected"

Preset

If no V3080As are connected both ALSO1 and ALSO2 are OFF.

If one V3080A is connected:

ALOS1 is F9_6

ALOS2 is OFF

If two V3080As are connected both ALSO1 and ALSO2 are F9_6.

State Saved

Yes

Initial S/W Revision

A.11.50

LF Out

For M9484C with Option AN1.

ClosedView image.

LF Out, Low Frequency Output, is a connector that provides function generator capability. This function generator is independent of the RF Output.

State

Enables, or disables, the output on the LF Out connector.

SCPI Command

[:SOURce][:RF<channel>]:LFOutput:STATe ON|OFF|1|0

[:SOURce][:RF<channel>]:LFOutput:STATe?

SCPI Example

LFO:STAT ON

LFO:STAT?

Notes

For M9484C without option AN1, attempting to set the state on will raise the error 703, Feature not supported; LF Out State unavailable, option AN1 is required.

For M9383B and M9384B, attempting to set state on will raise the error 703, Feature not supported; LF Out State unavailable on this instrument.

Preset

OFF

State Saved

Yes

Initial S/W Revision

A.11.50

Amplitude

This setting determines the amplitude of the signal at the LF Out connector. The total of DC Offset and amplitude cannot exceed the maximum amplitude value. If the source is DC, then only the DC Offset can be used. The value is for 50 Ohm load impedance.

SCPI Command

[:SOURce][:RF<channel>]:LFOutput:AMPLitude <voltage>

[:SOURce][:RF<channel>]:LFOutput:AMPLitude?

SCPI Example

LFO:AMPL 2V

LFO:AMPL?

Preset

0 V

State Saved

Yes

Min

0

Max

5 Vp

Resolution

0.001 V

Initial S/W Revision

A.11.50

DC Offset

This setting determines the DC Offset (in volts) of the signal at the LF Out connector. The total of DC Offset and amplitude cannot exceed the maximum amplitude value. If the source is DC, then only the DC Offset can be used. The value is for 50 Ohm load impedance.

SCPI Command

[:SOURce][:RF<channel>]:LFOutput:OFFSet <voltage>

[:SOURce][:RF<channel>]:LFOutput:OFFSet?

SCPI Example

LFO:OFFS -2V

LFO:OFFS?

Preset

0 V

State Saved

Yes

Min

-5 V

Max

5 V

Resolution

0.001 V

Initial S/W Revision

A.11.50

Source

This setting determines the source of the LF Out.

DC (DC) – Selects DC as the modulation source, which means that the LF Output DC Offset sets a continuous output voltage.

Function 1 (FUNCtion[1]) – Selects function generator 1 as the modulation source.

SCPI Command

[:SOURce][:RF<channel>]:LFOutput:SOURce DC|FUNCtion[1]

[:SOURce][:RF<channel>]:LFOutput:SOURce?

SCPI Example

LFO:SOUR DC

LFO:SOUR?

Preset

FUNC1

State Saved

Yes

Initial S/W Revision

A.11.50

Function 1

Frequency

Sets the frequency modulation rate for the waveform on the selected internal function generator.

SCPI Command

[:SOURce][:RF<channel>]:LFOutput:FUNCtion[1]|2:FREQuency <frequency>

[:SOURce][:RF<channel>]:LFOutput:FUNCtion[1]|2:FREQuency?

SCPI Example

LFO:FUNC:FREQ 30

LFO:FUNC:FREQ?

Preset

400 Hz

State Saved

Yes

Min

M9484C: 0.01 Hz

Max

1 MHz

M9484C: 10 MHz

Resolution

M9484C: 0.01 Hz

Initial S/W Revision

A.11.50

Frequency Increment

Remote command only.

Sets the step increment for the internal frequency.

SCPI Command

[:SOURce][:RF<channel>]:LFOutput:FREQuency:STEP[:INCRement] <frequency>

[:SOURce][:RF<channel>]:LFOutput:FREQuency:STEP[:INCRement]?

SCPI Example

LFO:FREQ:STEP 10 KHZ

LFO:FREQ:STEP?

Dependencies

Default value of 500 Hz is set by Restore System Defaults

Preset

500 Hz

State Saved

Persistent, survives preset and power cycle but not saved in the instrument state.

Min

M9484C: 0.01 Hz

Max

1 MHz

Resolution

M9484C: 0.01 Hz

Initial S/W Revision

A.11.50

Phase Offset

Sets the phase offset (in radians) of the output. The value can be set in degrees as well via both GUI and SCPI.

SCPI Command

[:SOURce][:RF<channel>]:LFOutput:FUNCtion[1]|2:POFFset <angle>

[:SOURce][:RF<channel>]:LFOutput:FUNCtion[1]|2:POFFset?

SCPI Example

LFO:FUNC:POFF 2

LFO:FUNC:POFF?

Preset

0

State Saved

Yes

Min

-6.29 rad

Max

6.29 rad

Resolution

0.001 rad

Initial S/W Revision

A.11.50

Shape

Sets the LF Output waveform type.

SCPI Command

[:SOURce][:RF<channel>]:LFOutput:FUNCtion[1]|2:SHAPe SINE|TRIangle|PULSe|RAMP

[:SOURce][:RF<channel>]:LFOutput:FUNCtion[1]|2:SHAPe?

SCPI Example

LFO:FUNC:SHAP SINE

LFO:FUNC:SHAP?

Preset

SINE

State Saved

Yes

Initial S/W Revision

A.11.50

Shape Ramp Polarity

Remote command only.

Sets the ramp direction when :LFOutput:FUNCtion[1]|2:SHAPe is set to RAMP.

SCPI Command

[:SOURce][:RF<channel>]:LFOutput:FUNCtion[1]|2:SHAPe:RAMP POSitive|NEGative

[:SOURce][:RF<channel>]:LFOutput:FUNCtion[1]|2:SHAPe:RAMP?

SCPI Example

LFO:FUNC:SHAP:RAMP NEG

LFO:FUNC:SHAP:RAMP?

Preset

POSitive

State Saved

Yes

Initial S/W Revision

A.11.50

Duty Cycle

Sets the duty cycle in percent for Pulse mode.

SCPI Command

[:SOURce][:RF<channel>]:LFOutput:FUNCtion[1]|2:DCYCle <real>

[:SOURce][:RF<channel>]:LFOutput:FUNCtion[1]|2:DCYCle?

SCPI Example

LFO:FUNC:DCYC 20

LFO:FUNC:DCYC?

Preset

50

State Saved

Yes

Min

0

Max

100

Resolution

0.000000000001

Initial S/W Revision

A.11.50

Global Trigger / Sync