NR-V2X

Carrier

Add Delete BWP or Channels

General

Enabled

Frequency Offset

Timing Offset

Power Boosting

Initial Phase

Spectrum Control

DC Punctured

Window Beta

Windowing Method

Baseband Filter

Cell-Specific

Cell ID

Bandwidth

Numerology

Max RB

K0

Configured Bandwidth

Frequency Offset of Point A

Base Sample Rate

Sidelink Setup

BWP Setup

Channel Setup: S-SS/PSBCH

Channel Setup: PSCCH

Channel Setup: PSSCH

Channel Setup: PFSCH

Channel Setup: CSI-RS

Add Delete BWP or Channels

User can add/delete BWP or channels of S-SS/PSBCH, PSCCH, PSSCH, CSI-RS, PSFCH. When delete channels or BWP, re-index will be done on the left channels or BWPs. Index/Cardinality of channel or BWP starts from 0, so valid index or cardinality range is from 0 to the channel count or  bwp count minus 1. User should NOT try to access channels or BWPs which do not exist.

General

Enabled

This setting specifies enable state of Carrier

SCPI Command

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>[:STATe]?

SCPI Example

RADio:NV2X:WAVeform:CCAR0:STAT OFF

RADio:NV2X:WAVeform:CCAR0:STAT?

Preset

ON

State Saved

No

Range

OFF|ON

Frequency Offset

This setting specifies the frequency offset to the carrier signal.

SCPI Command

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:FREQuency:OFFSet <freq>

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:FREQuency:OFFSet?[MAXimum|MINimum]

SCPI Example

RADio:NV2X:WAVeform:CCAR0:FREQ:OFFS 10MHZ

RADio:NV2X:WAVeform:CCAR0:FREQ:OFFS?

Preset

0 Hz

State Saved

Yes

Min

-4 GHz

Max

4 GHz

Resolution

1 Hz

Timing Offset

This setting specifies timing offset of carrier relative to others.

SCPI Command

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:TIMing:OFFSet <time>

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:TIMing:OFFSet?[MAXimum|MINimum]

SCPI Example

RADio:NV2X:WAVeform:CCAR0:TIM:OFFS 0.1 MS

RADio:NV2X:WAVeform:CCAR0:TIM:OFFS?

Preset

0 s

State Saved

Yes

Min

0 s

Max

0.01 s

Resolution

1 ns

Power Boosting

This setting specifies the power boosting of the carrier relative to others.

SCPI Command

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:POWer <rel_ampl>

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:POWer?[MAXimum|MINimum]   

SCPI Example

RADio:NV2X:WAVeform:CCAR0:POW 3

RADio:NV2X:WAVeform:CCAR0:POW?

Preset

0 dB

State Saved

Yes

Min

-40 dB

Max

40 dB

Resolution

0.01 dB

Initial Phase

This setting specifies initial phase of the Carrier signal in degree

SCPI Command

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:INITial:PHASe <real>

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:INITial:PHASe?[MAXimum|MINimum]   

SCPI Example

RADio:NV2X:WAVeform:CCAR0:INIT:PHAS 10

RADio:NV2X:WAVeform:CCAR0:INIT:PHAS?

Preset

0 deg

State Saved

Yes

Min

0 deg

Max

360 deg

Resolution

1 deg

Spectrum Control

DC Punctured

This setting controls whether DC is punctured in the final signal for the current Carrier.

SCPI Command

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:DC:PUNCtured[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:DC:PUNCtured[:STATe]?

SCPI Example

RADio:NV2X:WAVeform:CCAR0:DC:PUNC ON

RADio:NV2X:WAVeform:CCAR0:DC:PUNC?

Couplings

For Uplink carrier with transform precoding enabled in UL-SCH, DC Punctured is forced to Off.

Preset

OFF

State Saved

Yes

Window Beta

This setting is used to set the windowing length to smooth OFDM symbol transitions. The value of it is a kind of fraction of FFT length instead of percentage.

SCPI Command

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:WINDow:BETA <real>

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:WINDOW:BETA?[MAXimum|MINimum]

 

 

SCPI Example

RAD:NV2X:WAV:CCARrier0:WIND:BETA 0.1

RAD:NV2X:WAV:CCARrier0:WIND:BETA?

Couplings

Only available when Carrier type is downlink or uplink.

Preset

0.01

State Saved

Yes

Min

0

Max

0.5

Resolution

0.01

Windowing Method

This setting controls the windowing methods applied to OFDM symbol transitions.

SCPI Command

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:WINDow:METHod CENTer|STARt

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:WINDow:METHod?

SCPI Example

RADio:NV2X:WAVeform:CCAR0:WIND:METH STAR

RADio:NV2X:WAVeform:CCAR0:WIND:METH?

Couplings

Only available when Carrier type is downlink or uplink.

Preset

CENTer

State Saved

Yes

IVI Driver

 

Baseband Filter

It enables or disables banseband filter.

It is recommended to enable baseband filter to achieve a balance between ACPR and EVM performance.

SCPI Command

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:BFILter[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:BFILter[:STATe]?

SCPI Example

RADio:NV2X:WAVeform:CCAR0:BFIL OFF

RADio:NV2X:WAVeform:CCAR0:BFIL?

Couplings

Only available when Carrier type is downlink or uplink.

Preset

ON

State Saved

Yes

Cell-Specific

Cell ID

This setting specifies Cell ID .

SCPI Command

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:CIDentity <integer>

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:CIDentity?[MAXimum|MINimum]

SCPI Example

RADio:NV2X:WAVeform:CCAR0:CID 3

RADio:NV2X:WAVeform:CCAR0:CID?

Preset

0

State Saved

Yes

Min

0

Max

1007

Resolution

1

Bandwidth

This setting specifies the bandwidth configuration.

SCPI Command

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:BWIDth FR1BW5M|FR1BW10M|FR1BW15M|FR1BW20M|FR1BW25M|FR1BW30M|FR1BW40M|FR1BW50M|FR1BW60M|FR1BW70M|FR1BW80M|FR1BW90M|FR1BW100M|FR2BW50M|FR2BW100M|FR2BW200M|FR2BW400M

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:BWIDth?

SCPI Example

RADio:NV2X:WAVeform:CCAR0:BWID FR1BW60M

RADio:NV2X:WAVeform:CCAR0:BWID?

Preset

FR1BW100M

State Saved

Yes

Numerology

This setting specifies the numerology.

SCPI Command

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:SNUMerology MU0|MU1|MU2Ncp|MU2Ecp|MU3

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:SNUMerology?

SCPI Example

RADio:NV2X:WAVeform:CCAR0:SNUM MU0

RADio:NV2X:WAVeform:CCAR0:SNUM?

Couplings

It is coupled with Bandwidth.

When Bandwidth is  FR1 , then MU0 , MU1, MU2Ncp and MU2Ecp are valid values.

When Bandwidth is FR2 ,then MU2Ncp, MU2Ecp ,MU3 are valid values.

When Bandwidth is switched from FR2 to FR1, this setting will be coupled to MU0

When Bandwidth is switched from FR1 to FR2, this setting will be coupled to MU2

Preset

MU1

State Saved

Yes

Max RB

It specifies the maximum RB numbers.

SCPI Command

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:SNUMerology:RB:NUMBer <integer>

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:SNUMerology:RB:NUMBer?[MAXimum|MINimum]

SCPI Example

RADio:NV2X:WAVeform:CCAR0:SNUM:RB:NUMB 100

RADio:NV2X:WAVeform:CCAR0:SNUM:RB:NUMB?

Couplings

It is coupled with  Bandwidth, Numerology.

Maximum value depends on Numerology and Bandwidth, the maximum value is listed in the "Maximum Value" of  RB Number Table.

When switch Bandwidth, this setting will be coupled to the "standard value" listed in RB Number Table

Preset

273

State Saved

Yes

Min

6

Max

275

Resolution

1

K0

It specifies k0 which is used to adjust the center of carrier.

SCPI Command

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:SNUMerology:K0MU <real>

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:SNUMerology:K0MU?[MAXimum|MINimum]

SCPI Example

RADio:NV2X:WAVeform:CCAR0:SNUM:K0MU 6

RADio:NV2X:WAVeform:CCAR0:SNUM:K0MU?

Couplings

The valid values are -6,0,6.

Preset

0

State Saved

Yes

Min

-6

Max

6

Resolution

1

Configured Bandwidth

This setting is read only setting. It tells user the configured bandwidth of carrier and is calculated by the maximum bandwidth with current numerology.

SCPI Command

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:CBWidth?

SCPI Example

RADio:NV2X:WAVeform:CCAR0:CBW?

Preset

98.28 MHz

State Saved

Yes

Frequency Offset of Point A

It is read only setting and tells the relative location of Point A from the middle of the carrier.

SCPI Command

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:APOint:FREQuency:OFFSet?

SCPI Example

RADio:NV2X:WAVeform:CCAR0:APO:FREQ:OFFS?

Preset

-49.14 MHz

State Saved

Yes

Base Sample Rate

This is a read only setting. It specifies the current carrier’s sample rate which is calculated automatically.

SCPI Command

[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:SRATe?

SCPI Example

RADio:NV2X:WAVeform:CCAR0:SRAT?

Preset

122.88 MHz

Resolution

 

FRC Config

Tx Config

Waveform

Welcome to NR-V2X