Digital Video
Sets the format to be used. Currently, only DVB-S2/S2X format is supported.
DVB-S2/S2X (EN 302307) is introduced to improve the transmission capability in the same bandwidth as DVB-S. More complicated BCH and LDPC coding and high order modulation scheme such as QPSK, 8PSK, 16APSK and 32APSK are adopted.
|
SCPI Command |
[:SOURce]:RADio:DVIDeo:WAVeform:FORMat DVBSx [:SOURce]:RADio:DVIDeo:WAVeform:FORMat? |
|
SCPI Example |
|
|
Couplings |
|
|
Preset |
DVBSx |
|
State Saved |
Yes |
|
Initial S/W Revision |
A.20.01 |
|
SCPI Command |
[:SOURce]:RADio:DVIDeo:WAVeform:LVERsion:DATE:REQuired? |
|
SCPI Example |
|
|
Couplings |
|
|
Preset |
2026.0801 |
|
State Saved |
Yes |
|
Initial S/W Revision |
A.20.01 |
Enter an alpha-numeric comment up to 32 characters, in length. The comment resides in the file header and can include spaces and special characters.
|
SCPI Command |
[:SOURce]:RADio:DVIDeo:WAVeform:DVBSx:COMMent <string> [:SOURce]:RADio:DVIDeo:WAVeform:DVBSx:COMMent? |
|
SCPI Example |
|
|
Couplings |
|
|
Preset |
|
|
State Saved |
Yes |
|
Initial S/W Revision |
A.20.01 |
Query only
Displays the generated waveform length (number of points). This field is read-only.
|
SCPI Command |
[:SOURce]:RADio:DVIDeo:WAVeform:DVBSx:WLENgth? |
|
SCPI Example |
|
|
Couplings |
|
|
Preset |
0 |
|
State Saved |
Yes |
|
Min |
|
|
Max |
|
|
Initial S/W Revision |
A.20.01 |
Sets the oversampling ratio.
The value (number of points) is automatically determined based on the .
For example, considering is 696320 and ratio is 1, when ratio changed to 2, then becomes 696320*2 = 1392640.
|
SCPI Command |
[:SOURce]:RADio:DVIDeo:WAVeform:DVBSx:ORATio <integer> [:SOURce]:RADio:DVIDeo:WAVeform:DVBSx:ORATio? |
|
SCPI Example |
|
|
Couplings |
|
|
Preset |
2 |
|
State Saved |
Yes |
|
Min |
|
|
Max |
|
|
Initial S/W Revision |
A.20.01 |
Enables or disables the swapping of I and Q waveforms. This setting is used during the correction operation to account for low side upconversion between the signal generator and the spectrum analyzer.
|
SCPI Command |
[:SOURce]:RADio:DVIDeo:WAVeform:DVBSx:MSPectrum ON|OFF|1|0 [:SOURce]:RADio:DVIDeo:WAVeform:DVBSx:MSPectrum? |
|
SCPI Example |
|
|
Couplings |
|
|
Preset |
OFF |
|
State Saved |
Yes |
|
Initial S/W Revision |
A.20.01 |
Sets the baseband quadrature phase angle, in degrees.
Enter a value to adjust the Q phase angle. When the quadrature angle is zero, the phase angle between the I and Q vectors is 90 degrees. Positive angle adjustment increases the angle from 90 degrees while negative angle adjustment decreases the angle from 90 degrees.
|
SCPI Command |
[:SOURce]:RADio:DVIDeo:WAVeform:DVBSx:QAADjustment <real> [:SOURce]:RADio:DVIDeo:WAVeform:DVBSx:QAADjustment? |
|
SCPI Example |
|
|
Couplings |
|
|
Preset |
0 |
|
State Saved |
Yes |
|
Min |
|
|
Max |
|
|
Initial S/W Revision |
A.20.01 |
Sets the baseband quadrature gain balance, in dB.
Enter a gain ratio, by which I gain exceeds Q gain. For example, if you enter a value of 1 dB, the I signal will have 1 dB more amplitude than the Q signal.
Use the gain balance to remove imperfections in I and Q, or introduce calibrated impairments.
|
SCPI Command |
[:SOURce]:RADio:DVIDeo:WAVeform:DVBSx:IQGBalance <real> [:SOURce]:RADio:DVIDeo:WAVeform:DVBSx:IQGBalance? |
|
SCPI Example |
|
|
Couplings |
|
|
Preset |
0 |
|
State Saved |
Yes |
|
Min |
|
|
Max |
|
|
Initial S/W Revision |
A.20.01 |
Sets the Group setting that determines where the specific waveform of Digital Video is played.
|
SCPI Command |
[:SOURce]:RADio:DVIDeo:WAVeform:ROUTing:GROup <integer> [:SOURce]:RADio:DVIDeo:WAVeform:ROUTing:GROup? |
|
SCPI Example |
RADio:DVIDeo:WAVeform:ROUTing:GROup 1 RADio:DVIDeo:WAVeform:ROUTing:GROup? |
|
Couplings |
|
| Range | 0 - 7 |
|
Preset |
0 |
|
State Saved |
Yes |
|
Min |
|
|
Max |
|
|
Initial S/W Revision |
A.20.01 |
Sets the Signal setting that determines where the specific waveform of Digital Video is played.
|
SCPI Command |
[:SOURce]:RADio:DVIDeo:WAVeform:ROUTing:SIGNal <integer> [:SOURce]:RADio:DVIDeo:WAVeform:ROUTing:SIGNal? |
|
SCPI Example |
RADio:DVIDeo:WAVeform:ROUTing:SIGNal 1 RADio:DVIDeo:WAVeform:ROUTing:SIGNal? |
|
Couplings |
|
| Range | 0 - 7 |
|
Preset |
0 |
|
State Saved |
Yes |
|
Min |
|
|
Max |
|
|
Initial S/W Revision |
A.20.01 |