GNSS
GNSS is a real-time only application. You can turn the State On or Off by:
either using the State checkbox on the top bar.
or using the SCPI command.
When State is set to On, the following settings will be read-only.
Scenario Type
Orbit Data Type
Start Time (GPS Time)
GPS Almanac File
Galileo Almanac File
BeiDou Almanac File
QZSS Almanac File
GLONASS Almanac File
NavIC Almanac File
RINEX Files
NMEA Message File
Trajectory Mode
|
SCPI Command |
[:SOURce]:RADio:GNSS:WAVeform:STATe ON|OFF|0|1 [:SOURce]:RADio:GNSS:WAVeform:STATe? |
|
SCPI Example |
RADio: GNSS:WAVeform:STATe ON RADio: GNSS:WAVeform:STATe? |
|
Preset |
When you preset the instrument, the real-time GNSS application will be turned off. |
|
Initial S/W Revision |
A.16.00 |