Programming

This topic links to information on programming and remote operation of the VXG signal generator.

Getting Started with Remote Operation

provides information on remote operation, including the IO interfaces

SCPI for Signal Generation Applications

provides information on using SCPI for applications, such as 5G NR

Programming the Instrument

provides information about the instrument's SCPI programming interface and status registers

SCPI Basics

provides basic information about SCPI commands

SCPI Programming Examples

provides SCPI examples for common remote programming tasks

SCPI List

provides a comprehensive list of the SCPI commands with links to their descriptions

Marker Editing Using SCPI

describes the SCPI commands used for editing markers in non-volitile memory

Channel Bonding Temperature Compensation Using SCPI

describes the SCPI commands used for temperature compensation in channel bonding