Channel Studio TDL

General

This tab allows you to configure the basic information of the custom fading profile, such as:

The General tab has the following settings:

Fading Profile Name

Number Of Tx Antennas

Number Of Rx Antennas

Center Frequency Mode

Hardware RF Output Channel

Center Frequency

Initial Delay

Doppler Unit

Delay Unit

Distribution Seed

Delay Spread

Vehicle Speed

Fading Profile Name

Sets the name of the fading profile. The Channel Studio TDL application saves the fading profile (.tdlx) file with this name when you Generate the fading profile.

SCPI Command

[:SOURce]:RADio:CSTDl:FADing:PROFile:NAME

[:SOURce]:RADio:CSTDl:FADing:PROFile:NAME?

SCPI Example

 

Couplings

 

Preset

Untitled

State Saved

Yes

Initial S/W Revision

A.19.00

Number Of Tx Antennas

Sets the number of Tx Antennas of MIMO.

SCPI Command

[:SOURce]:RADio:CSTDl:FADing:PROFile:TX:ANTennas:COUNt <integer>

[:SOURce]:RADio:CSTDl:FADing:PROFile:TX:ANTennas:COUNt?

SCPI Example

 

Couplings

 

Preset

1

Choices 1 | 2 | 4 | 8

State Saved

Yes

Initial S/W Revision

A.19.00

Number Of Rx Antennas

Sets the number of Rx Antennas of MIMO.

SCPI Command

[:SOURce]:RADio:CSTDl:FADing:PROFile:RX:ANTennas:COUNt <integer>

[:SOURce]:RADio:CSTDl:FADing:PROFile:RX:ANTennas:COUNt?

SCPI Example

 

Couplings

 

Preset

1

Choices 1 | 2 | 4 | 8 | 16

State Saved

Yes

Initial S/W Revision

A.19.00

Modified S/W Version A.19.03 - Added 16 as the supported option

Center Frequency Mode

Sets the way to update the center frequency in fading profile.

SCPI Command

[:SOURce]:RADio:CSTDl:FADing:PROFile:FREQuency:CENTer:MODE AUTO|MANual

[:SOURce]:RADio:CSTDl:FADing:PROFile:FREQuency:CENTer:MODE?

SCPI Example

 

Couplings

 

Preset

AUTO

State Saved

Yes

Initial S/W Revision

A.19.00

Hardware RF Output Channel

If Center Frequency Mode is set to Auto, then this setting sets the hardware channel of your signal generator whose frequency value will be used as the center frequency of fading profile.

SCPI Command

[:SOURce]:RADio:CSTDl:FADing:PROFile:RF:OUTPut:CHANnel <integer>

[:SOURce]:RADio:CSTDl:FADing:PROFile:RF:OUTPut:CHANnel?

SCPI Example

 

Couplings

 

Preset

1

State Saved

Yes

Min

1

Max

32

Initial S/W Revision

A.19.00

Center Frequency

Sets the center frequency of fading profile.

SCPI Command

[:SOURce]:RADio:CSTDl:FADing:PROFile:FREQuency:CENTer <real>

[:SOURce]:RADio:CSTDl:FADing:PROFile:FREQuency:CENTer?

SCPI Example

 

Couplings

 

Preset

3500000000

State Saved

Yes

Min

100kHz

Max

100000000000

Initial S/W Revision

A.19.00

Initial Delay

Sets the time delay value added for each Path.

SCPI Command

[:SOURce]:RADio:CSTDl:FADing:PROFile:INITial:DELay <real>

[:SOURce]:RADio:CSTDl:FADing:PROFile:INITial:DELay?

SCPI Example

 

Couplings

 

Preset

0

State Saved

Yes

Min

0

Max

0.001

Initial S/W Revision

A.19.00

Doppler Unit

Sets the unit type to be used to define the max doppler. Four types of Doppler units are available - Hz, m/s, km/h, mph

If Unit type is Hz, then:

If Unit type is m/s, km/h, or mph, then:

SCPI Command

[:SOURce]:RADio:CSTDl:FADing:PROFile:DOPPler:UNIT HZ|MPS|KMH|MPH

[:SOURce]:RADio:CSTDl:FADing:PROFile:DOPPler:UNIT?

SCPI Example

 

Couplings

 

Preset

HZ

State Saved

Yes

Initial S/W Revision

A.19.00

Delay Unit

Sets the time unit of delay gap between adjacent paths when adding fading path. Unit to delay supports the following options:

SCPI Command

[:SOURce]:RADio:CSTDl:FADing:PROFile:DELay:UNIT NS|US|MS

[:SOURce]:RADio:CSTDl:FADing:PROFile:DELay:UNIT?

SCPI Example

 

Couplings

 

Preset

NS

State Saved

Yes

Initial S/W Revision

A.19.00

Distribution Seed

Sets a seed for channel fading model generation. If you want to give different seeds for random generators to get slightly different models, it can be done using this setting.

SCPI Command

[:SOURce]:RADio:CSTDl:FADing:PROFile:DISTribution:SEED <integer>

[:SOURce]:RADio:CSTDl:FADing:PROFile:DISTribution:SEED?

SCPI Example

 

Couplings

 

Preset

2100000000

State Saved

Yes

Min

0

Max

2100000000

Initial S/W Revision

A.19.00

Delay Spread

Displays Information of the current delay spread.

This setting is read-only and is available only when more than one paths are defined.

SCPI Command

[:SOURce]:RADio:CSTDl:FADing:PROFile:DELay:SPRead?

SCPI Example

 

Couplings

 

Preset

0

State Saved

Yes

Min

 

Max

 

Initial S/W Revision

A.19.00

Vehicle Speed

Sets the maximum doppler when the Doppler Unit setting is set to m/s, km/h, or mph.

This setting is available only when the Unit type is set to m/s, km/h, or mph.

SCPI Command

[:SOURce]:RADio:CSTDl:FADing:PROFile:SPEed <real>

[:SOURce]:RADio:CSTDl:FADing:PROFile:SPEed?

SCPI Example

 

Couplings

 

Preset

36

State Saved

Yes

Min

0

Max

720

Initial S/W Revision

A.19.00