Pulse Building
Read-only setting that indicates the required license version date.
|
SCPI Command |
[:SOURce]:RADio:PBUilding:WAVeform:LVERsion:DATe:REQuired? |
|
SCPI Example |
RADio:PBUilding:WAVeform:LVERsion:DATe:REQuired? |
|
Couplings |
|
|
Preset |
2025.0901 |
|
State Saved |
Yes |
|
Initial S/W Revision |
A.18.00 |
Selects a pattern to generate.
|
SCPI Command |
[:SOURce]:RADio:PBUilding:WAVeform:SELected:PATTern:GENerate [:SOURce]:RADio:PBUilding:WAVeform:SELected:PATTern:GENerate? |
|
SCPI Example |
RADio:PBUilding:WAVeform:SELected:PATTern:GENerate "Pattern 1" RADio:PBUilding:WAVeform:SELected:PATTern:GENerate? |
|
Couplings |
|
|
Preset |
Pattern 1 |
|
State Saved |
Yes |
|
Initial S/W Revision |
A.18.00 |
Enable auto sample rate to allow Pulse Building to select the sample rate used during signal generation. This is typically the maximum sample rate supported by the instrument. Manually setting the sample rate to a lower value can reduce the amount of IQ waveform memory used to generate the pattern. A lower sample rate reduces the intra-pulse modulation bandwidth too.
|
SCPI Command |
[:SOURce]:RADio:PBUilding:WAVeform:SRATe:AUTo ON|OFF|1|0 [:SOURce]:RADio:PBUilding:WAVeform:SRATe:AUTo? |
|
SCPI Example |
RADio:PBUilding:WAVeform:SRATe:AUTo ON RADio:PBUilding:WAVeform:SRATe:AUTo? |
|
Couplings |
|
|
Preset |
ON |
|
State Saved |
Yes |
|
Initial S/W Revision |
A.18.00 |
Sets the sample rate used to generate the pattern.
|
SCPI Command |
[:SOURce]:RADio:PBUilding:WAVeform:SRATe <real> [:SOURce]:RADio:PBUilding:WAVeform:SRATe? |
|
SCPI Example |
RADio:PBUilding:WAVeform:SRATe 3000000000 RADio:PBUilding:WAVeform:SRATe? |
|
Couplings |
|
|
Dependencies |
Auto Sample Rate must be disabled. Limits are hardware specific. |
|
Preset |
3 GHz |
|
State Saved |
Yes |
|
Min |
1 MHz |
|
Max |
For M9484C
|
|
Initial S/W Revision |
A.18.00 |
The signal bandwidth parameter serves two purposes: The first is to set the bandwidth of the test signal. The second is to help optimize signal corrections.
|
SCPI Command |
[:SOURce]:RADio:PBUilding:WAVeform:SBWidth:AUTo ON|OFF|1|0 [:SOURce]:RADio:PBUilding:WAVeform:SBWidth:AUTo? |
|
SCPI Example |
RADio:PBUilding:WAVeform:SBWidth:AUTo ON RADio:PBUilding:WAVeform:SBWidth:AUTo? |
|
Couplings |
|
|
Preset |
ON |
|
State Saved |
Yes |
|
Initial S/W Revision |
A.18.00 |
Set the value to the maximum RF bandwidth of your signal.
|
SCPI Command |
[:SOURce]:RADio:PBUilding:WAVeform:SBWidth <real> |
|
SCPI Example |
RADio:PBUilding:WAVeform:SBWidth 2400000000 RADio:PBUilding:WAVeform:SBWidth? |
|
Couplings |
|
|
Preset |
2.4 GHz |
|
State Saved |
Yes |
|
Min |
10 MHz |
|
Max |
For M9484C:
|
|
Initial S/W Revision |
A.18.00 |
This property is used to correct the RF spectrum when low side external frequency up/down conversion is used.
|
SCPI Command |
[:SOURce]:RADio:PBUilding:WAVeform:MSPectrum ON|OFF|1|0 [:SOURce]:RADio:PBUilding:WAVeform:MSPectrum? |
|
SCPI Example |
RADio:PBUilding:WAVeform:MSPectrum OFF RADio:PBUilding:WAVeform:MSPectrum? |
|
Couplings |
|
|
Preset |
OFF |
|
State Saved |
Yes |
|
Initial S/W Revision |
A.18.00 |
Sets the comments.
|
SCPI Command |
[:SOURce]:RADio:PBUilding:WAVeform:COMMent [:SOURce]:RADio:PBUilding:WAVeform:COMMent? |
|
SCPI Example |
RADio:PBUilding:WAVeform:COMMent "" RADio:PBUilding:WAVeform:COMMent? |
|
Couplings |
|
|
Preset |
|
|
State Saved |
Yes |
|
Initial S/W Revision |
A.18.00 |
Event marker indicates the first point at the start of a configured signal. A high transition, approximately + 2.5 VDC, indicates the beginning or start of the signal.
|
SCPI Command |
[:SOURce]:RADio:PBUilding:WAVeform:M1Source SSTart|PGATe|PSTart|NONe [:SOURce]:RADio:PBUilding:WAVeform:M1Source? |
|
SCPI Example |
RADio:PBUilding:WAVeform:M1Source NONe RADio:PBUilding:WAVeform:M1Source? |
|
Couplings |
|
|
Preset |
NONe |
|
State Saved |
Yes |
|
Initial S/W Revision |
A.18.00 |
Event marker is present during each pulse in a pattern. A high transition, approximately + 2.5 VDC, and time duration slightly longer than the pulse occurs for each pulse. This marker can be used as a trigger indicating that a pulse is about to be generated.
|
SCPI Command |
[:SOURce]:RADio:PBUilding:WAVeform:M2Source SSTart|PGATe|PSTart|NONe [:SOURce]:RADio:PBUilding:WAVeform:M2Source? |
|
SCPI Example |
RADio:PBUilding:WAVeform:M2Source NONe RADio:PBUilding:WAVeform:M2Source? |
|
Couplings |
|
|
Preset |
NONe |
|
State Saved |
Yes |
|
Initial S/W Revision |
A.18.00 |
Event marker indicates the start of a pulse. A high transition, approximately + 2.5 VDC, indicates the start of a pulse.
|
SCPI Command |
[:SOURce]:RADio:PBUilding:WAVeform:M3Source SSTart|PGATe|PSTart|NONe [:SOURce]:RADio:PBUilding:WAVeform:M3Source? |
|
SCPI Example |
RADio:PBUilding:WAVeform:M3Source NONe RADio:PBUilding:WAVeform:M3Source? |
|
Couplings |
|
|
Preset |
NONe |
|
State Saved |
Yes |
|
Initial S/W Revision |
A.18.00 |
Group setting determine where the specific waveform of Pulse Builder is played. The waveform file name will have a _G#S# suffix based on the routing configuration so user can specify different Group to generate/playback/edit this waveform.
|
SCPI Command |
[:SOURce]:RADio:PBUilding:WAVeform:ROUTing:GROup <integer> [:SOURce]:RADio:PBUilding:WAVeform:ROUTing:GROup? |
|
SCPI Example |
RADio:PBUilding:WAVeform:ROUTing:GROup 1 RADio:PBUilding:WAVeform:ROUTing:GROup? |
|
Couplings |
|
|
Preset |
1 |
|
State Saved |
Yes |
|
Min |
1 |
|
Max |
8 |
|
Initial S/W Revision |
A.18.00 |
Signal setting determine where the specific waveform of Pulse Builder is played. The waveform file name will have a _G#S# suffix based on the routing configuration so user can specify different Signal to generate/playback/edit this waveform.
|
SCPI Command |
[:SOURce]:RADio:PBUilding:WAVeform:ROUTing:SIGNal <integer> [:SOURce]:RADio:PBUilding:WAVeform:ROUTing:SIGNal? |
|
SCPI Example |
RADio:PBUilding:WAVeform:ROUTing:SIGNal 1 RADio:PBUilding:WAVeform:ROUTing:SIGNal? |
|
Couplings |
|
|
Preset |
1 |
|
State Saved |
Yes |
|
Min |
1 |
|
Max |
8 |
|
Initial S/W Revision |
A.18.00 |