To create a custom calibration kit that uses a new connector type, you must first define the connector family. The connector family is the name of the connector-type of the calibration kit, such as:
APC7
2.4 mm
Type-N (50Ω)
Although more than one connector family is allowed, it is best to limit each calibration kit to only one connector family.
If you are using a connector family that has male and female connectors, include definitions of both genders. If you are using a family with no gender, such as APC7, only one connector definition is required.
Use the following steps to create a custom calibration kit:
Press Cal > Cal Sets & Cal Kits > Cal Kit...
At the Manage Cal Kit dialog box, click Edit Kit....
In the Connectors Tab, click Add to name the new connector family.
Enter the Kit Description for the custom cal kit.
Click Add in the Connectors section of the dialog box.
Enter a Connector Family name.
Enter a Description of the connector.
Select the Gender of one of the connectors.
Enter the minimum and maximum Frequency Range.
Enter the Impedance.
Click the down-arrow to select the Media.
Enter the cut-off frequency
Click Apply.
Click OK.
If you need to add another connector gender, in the Connectors Tab, click Add in the Connectors section again for the next connector gender.
If you are adding another connector gender, repeat step 3.
Note: If you have male and female versions of the connector family, you probably do NOT also have a NO GENDER version.
Now that the connector family is added to the custom cal kit, you are ready to add new calibration standards.
In the Standards Tab, under the list of standards, click Add.
Select the type of standard (OPEN, SHORT, LOAD, or THRU), then click OK.
Complete the information in the dialog box for the standard you selected. Note that for banded standards, the start and stop frequency may be different than the frequency range of the specified connector. Edit the start and stop frequencies as needed. Click OK when all the settings are correct.
Repeat steps 2 - 3, as necessary, to add all standards and definitions to the new custom cal kit.
Assign each of the standards to a calibration class. This is done through the TRL Tab or SOLT Tab
Save the Cal Kit.
Last modified:
|
21-Aug-2014 |
First Release |