VNA firmware updates are available to you at no cost in a self-extracting Install Shield file. The update includes the VNA application, Online help, and Service Utilities..
To manually check the version of firmware on the VNA, click System > Help > About NA....
Tip: Use Move App to Back to cause the VNA application to move behind this application on the screen.
|
Note: After a firmware update...
|
Download the latest firmware from .
Terminate the VNA application by pressing System > Main > Exit.
Transfer the file from your PC to your VNA using LAN or USB Pen drive.
Double-click the file on the VNA and follow the instruction.
Warning: You can save the update file to your PC, but do not attempt to install the VNA application on your PC. It will alter system settings and can result in system crashes.
Last Modified:
|
18-May-2016 |
First release |