The file format for each user-defined antenna file consists of two parts: a parameter description section and a data section. For configurations containing multiple antennas, each antenna’s pattern must be saved in a separate ascii text file.
Sample Antenna File in Real-imaginary Format
The parameter description section defines the parameters and ranges for the data section entries.
|
|
begin_<parameters>
format free // can be others in the future for extension
phi_min 0 // the minimum phi angle to save in the file
phi_max 360 // the maximum phi angle to save in the file
phi_inc 5 // the increasing step for phi, the phi sampling points should be equal separation
theta_min 0 // the minimum theta angle to save in the file
theta_max 180 // the maximum theta angle to save in the file
Note: Although the file format is designed for a 3D pattern, it also supports a 2D pattern. For a 2D pattern, theta_min and theta_max should have the same value.
theta_inc 5 // the increment size for phi; the theta sampling points should have equal separation
complex // antenna gain must always be complex when used with the PXB, expressed either in magnitiude, phase format or real, imaginary format
mag_phase // the data file is given in magnitude - phase format
pattern gain // pattern must always be expressed in units of gain when used with the PXB
magnitude dB // magnitude is given in linear or in dB
direction degrees //phi and theta are given in degrees or radians
phase degrees // phase is given in degrees or in radians
polarization theta_phi // polarization type, theta_phi means vertical and horizontal polarization. It is the only polarization type currently supported with the PXB.
NetInputPower 0.002482195 // this parameter is not used in the current code
end_<parameters>
The data section follows the parameter section.
If the complex data is given as “mag_phase” type, the data should be in the following order:
Theta-angle // degrees or radians, determined by parameter “direction”
Phi-angle // degrees or radians, determined by parameter “direction”
Theta-gain // dB or linear, determined by parameter “magnitude”
Phi-gain // dB or linear, determined by parameter “magnitude”
Theta-Phase // degrees or radians, determined by parameter “phase”
Phi-Phase //degrees or radians, determined by parameter “phase”
If the complex data is given as real_imag type, the data should be in the following order:
Theta-angle //degrees or radians, determined by parameter “direction”
Phi-angle //degrees or radians, determined by parameter “direction”
Real part of Theta-gain
Imaginary part of Theta-gain
Real part of Phi-gain
Imaginary part of Phi-gain
The following sample file is in real-imaginary format.
begin_<parameters>
format free
phi_min 0
phi_max 350
phi_inc 10
theta_min 0
theta_max 0
theta_inc 5
complex
real_imag
pattern gain
magnitude dB
maximum_gain 0
phase degrees
direction degrees
polarization theta_phi
end_<parameters>
Note: The column headings below are shown for illustration purpose only. Do not include the headings in the actual antenna pattern file.
|
Theta Angle |
Phi Angle |
Theta Gain (real) |
Theta Gain (imag) |
Phi Gain (real) |
Phi Gain (imag) |
|
90.00000000 |
0.00000000 |
-0.43842839 |
-0.15259129 |
0.00000000 |
0.00000000 |
|
90.00000000 |
10.00000000 |
-0.42572635 |
0.01026539 |
0.00000000 |
0.00000000 |
|
90.00000000 |
20.00000000 |
-0.32281088 |
0.11955827 |
0.00000000 |
0.00000000 |
|
90.00000000 |
30.00000000 |
-0.20777300 |
0.29970148 |
0.00000000 |
0.00000000 |
|
90.00000000 |
40.00000000 |
-0.04687369 |
0.34673489 |
0.00000000 |
0.00000000 |
|
90.00000000 |
50.00000000 |
0.10793167 |
0.33498567 |
0.00000000 |
0.00000000 |
|
90.00000000 |
60.00000000 |
0.20787062 |
0.28438604 |
0.00000000 |
0.00000000 |
|
90.00000000 |
70.00000000 |
0.29245327 |
0.18851474 |
0.00000000 |
0.00000000 |
|
90.00000000 |
80.00000000 |
0.33242605 |
0.11528605 |
0.00000000 |
0.00000000 |
|
90.00000000 |
90.0000000 |
0 0.31069331 |
0.00483315 |
0.00000000 |
0.00000000 |
|
90.00000000 |
100.00000000 |
0.31012726 - |
0.10480700 |
0.00000000 |
0.00000000 |
|
90.00000000 |
110.00000000 |
0.30912890 |
-0.13342457 |
0.00000000 |
0.00000000 |
|
90.00000000 |
120.00000000 |
0.28879046 - |
0.14533395 |
0.00000000 |
0.00000000 |
|
90.00000000 |
130.00000000 |
0.30746698 - |
0.12487962 |
0.00000000 |
0.00000000 |
|
90.00000000 |
140.00000000 |
0.32104099 |
-0.07518822 |
0.00000000 |
0.00000000 |
|
90.00000000 |
150.00000000 |
0.36193118 - |
0.00451717 |
0.00000000 |
0.00000000 |
|
90.00000000 |
160.00000000 |
0.34073040 |
0.12281265 |
0.00000000 |
0.00000000 |
|
90.00000000 |
170.00000000 |
0.29552690 |
0.2081678 |
0.00000000 |
0.00000000 |
|
90.00000000 |
180.00000000 |
0.17650749 |
0.26925028 |
0.00000000 |
0.00000000 |
|
90.00000000 |
190.00000000 |
-0.01919988 |
0.26765785 |
0.00000000 |
0.00000000 |
|
90.00000000 |
200.00000000 |
-0.17468492 |
0.25349524 |
0.00000000 |
0.00000000 |
|
90.00000000 |
210.00000000 |
-0.25899719 |
0.17498510 |
0.00000000 |
0.00000000 |
|
90.00000000 |
220.00000000 |
-0.28185054 |
0.02505896 |
0.00000000 |
0.00000000 |
|
90.00000000 |
230.00000000 |
-0.26443563 |
-0.11240494 |
0.00000000 |
0.00000000 |
|
90.00000000 |
240.00000000 |
-0.20053945 |
-0.24269219 |
0.00000000 |
0.00000000 |
|
90.00000000 |
250.00000000 |
-0.16019569 |
-0.34511054 |
0.00000000 |
0.00000000 |
|
90.00000000 |
260.00000000 |
-0.10266138 |
-0.37629325 |
0.00000000 |
0.00000000 |
|
90.00000000 |
270.00000000 |
-0.01982612 |
-0.39305047 |
0.00000000 |
0.00000000 |
|
90.00000000 |
280.00000000 |
0.05068323 |
-0.43427250 |
0.00000000 |
0.00000000 |
|
90.00000000 |
290.00000000 |
0.07466213 |
-0.48400809 |
0.00000000 |
0.00000000 |
|
90.00000000 |
300.00000000 |
0.05858757 |
-0.52089012 |
0.00000000 |
0.00000000 |
|
90.00000000 |
310.00000000 |
0.00684469 |
-0.55631056 |
0.00000000 |
0.00000000 |
|
90.00000000 |
320.00000000 |
-0.05999220 |
-0.50553610 |
0.00000000 |
0.00000000 |
|
90.00000000 |
330.00000000 |
-0.12638610 |
-0.47581672 0. |
0.00000000 |
0.00000000 |
|
90.00000000 |
340.00000000 |
0.28591476 |
-0.40821738 |
0.00000000 |
0.00000000 |
|
90.00000000 |
350.00000000 |
-0.29630187 |
-0.39917608 |
0.00000000 |
0.00000000 |