Multiprobe channel models are represented by one or more clusters. Depending on the probe settings and the channel model, different power weights are assigned to the probes per cluster. This read-only table shows these assignments.
The Cluster Weighting tab replaces the Power Imbalance tab when a multiprobe MIMO OTA (e.g., Ring of Probes Method) channel model is selected.