The following waveform files are provided with the PXB for you use. The folder containing these files is: C:\<Program Files for Win XP><Program Files (x86) for Win 7>\Agilent\PXB\FactoryDefaultWaveforms
The following is a description of each waveform file.
|
File Name |
Description |
|
2TONE_WFM.SECUREWAVE |
2 sine wave tones, 1 MHz separation |
|
12TONE_WFM.SECUREWAVE |
12 sine wave tones, 400 kHz separation |
|
CDMA2K_9CHAN_WFM.SECUREWAVE |
cdma2000, FWD 9 Chan, IS-95A ACP EQ, 1 Carrier |
|
CDMA2K_PILOT_WFM.SECUREWAVE |
cdma2000, FWD Pilot, IS-95A EVM EQ, 1 Carrier |
|
default1.bin |
5000 samples, one cycle of a sine wave - |
|
default2.bin |
5000 samples, two cycles of a sine wave - |
|
default3.bin |
5000 samples, three cycles of a sine wave - |
|
default4.bin |
5000 samples, four cycles of a sine wave - |
|
defaultMarker.bin |
This file is not
a waveform file; it is a 5000 sample marker file that is intended to be
used with waveform files: default1.bin, default2.bin, default3.bin, and
default4.bin |
|
EDGE_1C_CONT_WFM.SECUREWAVE |
EDGE, Continuous Modulation, 1 Carrier |
|
EDGE_1C_BURST_WFM.SECUREWAVE |
EDGE, 1 8PSK Normal (PN15) Timeslot, 1 Carrier |
|
GSM_1C_BURST_WFM.SECUREWAVE |
GSM, 1 GMSK Normal (PN15) Timeslot, 1 Carrier |
|
GSM_1C_CONT_WFM.SECUREWAVE |
GSM, Continuous Modulation, 1 Carrier |
|
LTE_DL_03_2008.wfm |
Version of 3GPP Standard: March
2008 |
|
1M_MULTI-TONE |
Multi-tone waveform, 1 MHz tone spacing |
|
QAM16_WFM.SECUREWAVE |
16QAM, α=0.25 RNYQ, 4 Msps, 1 Carrier |
|
QPSK_WFM.SECUREWAVE |
QPSK, α=0.25 RNYQ, 4 Msps, 1 Carrier |
|
RAMP_TEST_WFM_2.bin |
400 Samples containing two ramps - |
|
SINE_TEST_WFM_2.bin |
The waveform is a single tone that appears on the low side of the carrier. With a frequency of –(sample rate)/200. For a sample rate of 100 MHz the tone appears 500 kHz below the carrier frequency. This is a copy of the SINE_TEST_WFM waveform found in the ESG and MXG. The waveform was copied twice to meet the PBX minimum size requirement (256 samples). |
|
WCDMA_1DPCH_WFM.SECUREWAVE |
W-CDMA, DL 1 DPCH, 1 Carrier |
|
WCDMA_TM1_64DPCH_1C_WFM.SECUREWAVE |
W-CDMA, DL TM1 + 64 DPCH, 1 Carrier |
|
WCDMA_TM1_64DPCH_4C_WFM.SECUREWAVE |
W-CDMA, DL TM1 + 64 DPCH, 4 Carriers |
|
WiMAX_10 MHz_1024 FFT.wfm |
One frame containing one DL-PUSC zone which
includes the basic MAC messages needed for receiver test (DL-MAP, UL-MAP,
DCD, and UCD), followed by 3 data bursts, all with QPSK (CTC) ½ modulation
and coding. The important system parameters for
demodulation are: |
|
WIMAX_10MHZ_64QAM_WFM.SECUREWAVE |
WiMAX™, 1024FFT, DL, PUSC, 30 SYM, 64QAM, 10 MHz BW |
|
WIMAX_10MHZ_QPSK_WFM.SECUREWAVE |
WIMAX, 1024FFT, DL, PUSC, 30 SYM, QPSK, 10 MHz BW |
|
WLAN20MHZ54M64QAM_WFM.SECUREWAVE |
WLAN, OFDM 64QAM, 54 Mbps, 20 MHz BW |