Displays the slot in which the board is located.
Baseband Gen/Fader cards are placed in slots 0 through 5 inside the PXB.
I/O cards are placed in slots A through D at the rear panel of the PXB. These slots are labeled on the rear panel from top to bottom.
Displays the name and description of the PXB assembly.
Displays the order fulfillment code of the assembly. (This code is for internal use only. You may be asked for this code by your Agilent representative if the PXB is suspected of having a hardware problem.)
Displays the hardware revision ID code of the assembly. (This code is for internal use only. You may be asked for this code by your Agilent representative if the PXB is suspected of having a hardware problem.)