The Agilent IO Libraries Suite includes four IO Libraries that allow you to programmatically control instruments, send commands to them, and receive responses and data. The Agilent IO Libraries Suite Online Help provides guidelines to help you choose among these libraries; in general, VISA and VISA COM are recommended for new development. The IO libraries are included with GPIB interface cards, or can be downloaded from the National Instruments website or the Agilent website. The Agilent IO Libraries are pre-installed on the PXB at shipment.
The Agilent IO Libraries Suite includes a number of utilities to help you connect, configure, and troubleshoot your test system, such as, Connection Expert, Event Viewer, Interactive IO, VISA Assistant, and IO Monitor. The IO Libraries Suite Connectivity Guide, available from the Agilent website or by right-clicking the IO icon in the lower task bar after installing the libraries, gives detailed help on connecting instruments using GPIB, LAN or USB interfaces.
To write programs to control your PXB, an IO library must be installed on a computer and the computer configured for instrument control using the GPIB interface. The following is a description of IO libraries available when using GPIB for instrument connection.
|
VISA
|
VISA is an IO library used to develop IO applications and instrument drivers that comply with industry standards. The NI-VISA and Agilent VISA libraries are similar implementations of VISA and have the same commands, syntax, and functions. The differences are in the lower level IO libraries; NI-488.2 and SICL respectively. It is best to use the Agilent VISA library with the Agilent GPIB interface card or NI-VISA with the NI PCI-GPIB interface card. |
||
|
SICL |
Agilent SICL can be used without the VISA overlay. The SICL functions can be called from a program. However, if this method is used, executable programs will not be portable to other hardware platforms. For example, a program using SICL functions will not run on a computer with NI libraries (PCI-GPIB interface card).
|
||
|
NI-488.2
|
NI-488.2 can be used without the VISA overlay. The NI-488.2 functions can be called from a program. However, if this method is used, executable programs will not be portable to other hardware platforms. For example, a program using NI-488.2 functions will not run on a computer with Agilent SICL (Agilent GPIB interface card). |
To write programs to control your PXB, an IO library must be installed on your computer and the computer configured for instrument control using the LAN interface. The following is a description of IO libraries available when using LAN for instrument connection.
VISA | VISA is an IO library used to develop IO applications and instrument drivers that comply with industry standards. Use the Agilent VISA library for programming the PXB over the LAN interface. |
SICL | Agilent SICL is a lower level library that is installed along with Agilent VISA. |
Along with Standard Commands for Programming Instructions (SCPI) and IO library functions, you can use a programming language to remotely control the PXB. Any programming language that can send commands using Telnet LAN on port 5024 or Socket LAN on port 5025 can be used.
| The PXB’s USB interface requires Agilent IO Libraries Suite 15.0 or later to run properly. |
To write programs to control your PXB, an IO library must be installed on your computer and the computer configured for instrument control using the USB interface. The following is a description of IO libraries available when using USB for instrument connection.
VISA | VISA is an I/O library used to develop I/O applications and instrument drivers that comply with industry standards. It is recommended that the VISA library be used for programming the PXB. The NI-VISA and Agilent VISA libraries are similar implementations of VISA and have the same commands, syntax, and functions. The differences are in the lower level I/O libraries used to communicate over the USB; NI-488.2 and SICL respectively. | ||
VISA COM | VISA COM is a COM (Microsoft Common Object Model) implementation based on the Agilent VISA architecture. | ||
NI-488.2 | NI-488.2 IO libraries can be used to develop applications for the USB interface. Refer to National Instrument’s website for information on NI-488.2. | ||
SICL | Agilent SICL can be used to develop applications for the USB interface. Refer to Agilent’s website for information on SICL.
|