The LTE Moving Propagation condition tests
a receiver’s ability to adjust to changing delay conditions. The
ETU200 profile uses multiple paths (taps) and is based on a 200 Hz doppler
frequency.
Illustration...
The AWGN Only profile uses a single path with a doppler frequency of 622.653 Hz.
|
|
When you select Moving Propagation in the Master Setup view as the fader profile, Delay, Min Delay, Max Delay and Rate of Oscillation can be set in the fader path columns. |
|
Parameter |
ETU 200 |
AWGN Only |
|
UE speed |
120 km/h |
350 km/h |
|
|
Normal |
Normal |
|
|
|
|
|
A |
10 µs |
10 µs |
|
|
0.04 s-1 |
0.13 s-1 |