The Precoding Matrix becomes visible as a tab in the Master Setup node in MIMO configurations after selecting a Single Stream, Dual Stream, or Static Orthogonal fading channel model.
These channel models conform to 3GPP TS 34.121-1 sections D.2.9.1, D.2.9.2, and D.2.9.3, and they are not editable.