These commands configure the Digital Signal Interface Module (DSIM) when it is assigned as an external instrument.
Numerical Choices:
DSIM[1]2|3|4 – These choices correspond to the number of DSIMs being used. If only one DSIM is used, regardless of the I/O port where it is connected, the DSIM will be DSIM1 in SCPI.
:CONTrol:DSIM[1]2|3|4[:EXTernal]:CLOCk:CPSample ONE|TWO|FOU
:CONTrol:DSIM[1]2|3|4[:EXTernal]:CLOCk:CPSample?
This command sets the number of clock cycles per sample output by the N5102A Digital Interface. When you select a number of clocks per sample that is greater than one, the sample is held for the selected number of clock cycles. This reduces the sample rate relative to the clock rate by a factor equal to the clocks per sample value.
This command is only valid when the Port Connection is Parallel.
:CONTrol:DSIM[1]2|3|4[:EXTernal]:CLOCk:OSRate <val>
:CONTrol:DSIM[1]2|3|4[:EXTernal]:CLOCk:OSRate?
This command sets the output sample rate for the DSIM. The available range for the output sample rate depends on the Port Configuration settings and is limited by the maximum clock rate. Changing the Clock Rate, Clocks per Sample, or Port Configuration will cause this value to be recalculated. This sample rate is matched to the IO output sample rate when the configuration is loaded and cannot be changed during runtime.
The value <val> is expressed in Hz.
Range: 1000 to 200E+06
:CONTrol:DSIM[1]2|3|4[:EXTernal]:CLOCk:PHASe D0|D90|D180|D270
:CONTrol:DSIM[1]2|3|4[:EXTernal]:CLOCk:PHASe?
This command adjusts the clock phase in 90-degree increments to 0, 90, 180, or 270 degrees. This value is runtime adjustable while the waveform is playing.
:CONTrol:DSIM[1]2|3|4[:EXTernal]:CLOCk:POLarity POSitive|NEGative
:CONTrol:DSIM[1]2|3|4[:EXTernal]:CLOCk:POLarity?
This command sets the alignment for the clock signal to positive or negative. This value is runtime adjustable while the waveform is playing.
|
POSitive |
This choice sets the sample alignment to occur on the rising edge transition of the clock signal. |
|
NEGative |
This choice sets sample alignment to occur on the falling edge transition of the clock signal. The Negative selection functions the same as setting the clock phase to 180 degrees. |
:CONTrol:DSIM[1]2|3|4[:EXTernal]:CLOCk:RATE <val>
:CONTrol:DSIM[1]2|3|4[:EXTernal]:CLOCk:RATE?
This command sets the clock rate at the user or DUT side of the N5102A digital interface module. This includes all effects on the clock such as serialization, and interleaving. Because of these settings, the clock rate can be different from the sample rate. Changing the Port Configuration will cause this value to be recalculated. This value is runtime adjustable while the waveform is playing.
The variable <val> is a expressed in Hz.
Range: 1kHz to 200 MHz (10E+06 if clock source is set to internal)
:CONTrol:DSIM[1]2|3|4:[EXTernal]:CLOCk:REFerence:FREQuency <val>
:CONTrol:DSIM[1]2|3|4:[EXTernal]:CLOCk:REFerence:FREQuency?
This command allows you to specify the frequency of the external reference supplied to the Freq Ref connector. This command is valid only when the clock source is set to internal. If this command is executed when the clock source is not set to internal, the parameter value is changed, but it is not used until the clock source is changed to internal.
Because a query returns the currently set value, regardless of the clock source, you must query both states (reference frequency and clock source) to know the current setup.
The variable <val> is expressed Hz.
Range: 1 kHz to 100 MHz
:CONTrol:DSIM[1]2|3|4[:EXTernal]:CLOCk:REFerence:SOURce INTernal|EXTernal
:CONTrol:DSIM[1]2|3|4[:EXTernal]:CLOCk:REFerence:SOURce?
This command sets the clock reference source to internal or external.
|
INTernal |
The N5102A digital interface module generates the sample clock. |
|
EXTernal |
The N5102A digital interface uses a clock provided by an external source through the Ext Clock In connector. The external clock is also available to the DUT at the Ext Clock Out connector. |
:CONTrol:DSIM[1]2|3|4[:EXTernal]:CLOCk:SKEW <val>
:CONTrol:DSIM[1]2|3|4[:EXTernal]:CLOCk:SKEW?
This command provides a fine-adjustment for aligning the clock to the valid portion of the data. Because this is a fine adjustment, it provides greater benefit at higher clock rates.
The maximum range for this value is +/- 5 nS, but the actual range depends on the clock rate. The clock skew value will be rounded to a resolution of 1/sample rate and is only active when the clock rate is greater than 25 MHz. If the sample rate is changed, the clock skew will adjust based on the previous number of samples skewed. This value is runtime adjustable while the waveform is playing.
The variable <val> is expressed in nanoseconds.
Range: –5 to 5
:CONTrol:DSIM[1]2|3|4[:EXTernal]:CLOCk:SOURce INTernal|EXTernal|DEVice
:CONTrol:DSIM[1]2|3|4[:EXTernal]:CLOCk:SOURce?
This command selects one of three possible clock sources.
|
INTernal |
With this choice, the N5102A digital interface module generates the sample clock. When the clock source is internal, both Reference Frequency and Frequency Reference Source become active. |
|
EXTernal |
With this choice, the N5102A digital interface uses a clock provided by an external source through the Ext Clock In connector. The external clock is also available to the DUT at the Ext Clock Out connector. |
|
DEVice |
With this choice, the DUT provides the clock to the N5102A digital interface through a pin on the breakout board connector ribbon cable. See the N5102A Digital Signal Interface Module Installation Guide for information about breakout boards. |
:CONTrol:DSIM[1]2|3|4[:EXTernal]:DATA:ALIGnment LSB|MSB
:CONTrol:DSIM[1]2|3|4[:EXTernal]:DATA:ALIGnment?
This command selects the bit alignment of words smaller than 16 bits to begin at either boundary of the data bus. The word alignment is coupled with the word size and the word order. This command is only valid in parallel mode. The Data Format Graph in the user interface updates to reflect changes to this selection.
|
LSB |
With this choice, the data will be aligned with the left data boundary (data line zero) for both I and Q. |
|
MSB |
With this choice, the data will be aligned with the right data boundary (data line 15) for both I and Q. |
:CONTrol:DSIM[1]2|3|4[:EXTernal]:DATA:BORDer LSB|MSB
:CONTrol:DSIM[1]2|3|4[:EXTernal]:DATA:BORDer?
This command selects the bit order for data transmitted through the N5102A module. In serial mode, data can be in least significant (LSB) bit first or most significant (MSB) bit first (data line zero). In parallel mode, you can assign the bit order of the data words to either the lowest or highest lines of the data word. The Data Format Graph in the user interface updates to reflect changes to this selection.
|
LSB |
With this choice, for a serial port configuration, the LSB of the data will be the first bit (data line zero) in a sample. In parallel or parallel interleaved port configuration, the LSB of the data word will appear on the lowest lines of the data word. |
|
MSB |
For a serial port configuration, the MSB will be the first bit in a sample. In parallel or parallel interleaved port configuration, the MSB of the data word will appear on the lowest lines of the data word. |
:CONTrol:DSIM[1]2|3|4[:EXTernal]:DATA:DIRection?
This query returns the direction for the data flow through the N5102A digital module according to the current I/O hardware configuration setup.
:CONTrol:DSIM[1]2|3|4[:EXTernal]:DATA:FRAMe:POLarity POSitive|NEGative
:CONTrol:DSIM[1]2|3|4[:EXTernal]:DATA:FRAMe:POLarity?
This command selects the polarity of the frame marker for serial transmission. The frame marker indicates the beginning of each sample or byte of data. The command is valid for serial transmission only.
|
POSitive |
This choice selects a positive polarity. The frame marker is high for the first data sample. |
|
NEGative |
This choice selects a negative polarity. The frame marker is low for the first data sample. |
:CONTrol:DSIM[1]2|3|4[:EXTernal]:DATA:INEGate ON|OFF|1|0
:CONTrol:DSIM[1]2|3|4[:EXTernal]:DATA:INEGate?
This command enables or disables negation of the value of each sample of the 'I' data. Negation changes the affected sample by expressing it in two's complement form, multiplying by negative one, and converting back to the selected numeric format. Negation can be done for I samples, Q samples, or both. The setting is runtime adjustable while the waveform is playing.
:CONTrol:DSIM[1]2|3|4[:EXTernal]DATA:IQ:POLarity POSitive|NEGative
:CONTrol:DSIM[1]2|3|4[:EXTernal]:DATA:IQ:POLarity?
This command selects the logic level for I and Q data. This value is runtime adjustable while the waveform is playing.
|
POSitive |
Selects a high logic level at the output as a digital one. |
|
NEGative |
Selects a low logic level at the output as a digital one. |
:CONTrol:DSIM[1]2|3|4:[EXTernal]:DATA:IQ:SWAP ON|OFF|1|0
:CONTrol:DSIM[1]2|3|4[:EXTernal]:DATA:IQ:SWAP?
This command enables or disables swapping of the I and Q data. When enabled, the 'I' data is sent to the N5102A's Q bus and the 'Q’ data is sent to the I bus. The setting may be changed while the waveform is playing.
:CONTrol:DSIM[1]2|3|4[:EXTernal]:DATA:NFORmat OBINary|TCOMplement
:CONTrol:DSIM[1]2|3|4[:EXTernal]:DATA:NFORmat?
This command selects the binary format used to represent the transmitted data values. This value is runtime adjustable while the waveform is playing.
|
OBINary |
This choice sets the N5102A module data format to an offset binary representation of the data values. |
|
TCOMplement |
This choice sets the N5102A module data format to a two’s complement representation of the data values. |
:CONTrol:DSIM[1]2|3|4[:EXTernal]:DATA:QNEGate ON|OFF|1|0
:CONTrol:DSIM[1]2|3|4[:EXTernal]:DATA:QNEGate?
This command enables or disables negation of the
value of each sample of the Q data. Negation changes the affected sample
by expressing it in two's complement form, multiplying by negative one,
and converting back to the selected numeric format. Negation can be done
for I samples, Q samples, or both. The setting is runtime adjustable while
the waveform is playing.
:CONTrol:DSIM[1]2|3|4[:EXTernal]:DATA:SIZE <val>
:CONTrol:DSIM[1]2|3|4[:EXTernal]:DATA:SIZE?
This command sets the number of bits in each sample transmitted through the N5102A module. A word is defined as an integer number of bits from 4 to 16. For parallel and parallel interleaved data, word is synonymous with sample. Any unused data lines are driven low. The word size is coupled with word alignment.
Range: 4
to 16
:CONTrol:DSIM[1]2|3|4[:EXTernal]:LOGic:TYPE LVDS|LVTTL|CMOS33|CMOS25|CMOS18|CMOS15
:CONTrol:DSIM[1]2|3|4[:EXTernal]:LOGic:TYPE?
This command selects the logic data type used by the device being tested.
|
LVDS |
This choice selects low voltage differential signaling as the logic data type. |
|
LVTTL |
This choice selects a low voltage TTL signal as the logic data type. |
|
CMOS33 |
This choice selects a 3.3 volt CMOS signal as the logic data type. |
|
CMOS25 |
This choice selects a 2.5 volt CMOS signal as the logic data type. |
|
CMOS18 |
This choice selects a 1.8 volt CMOS signal as the logic data type. |
|
CMOS15 |
This choice selects a 1.5 volt CMOS signal as the logic data type. |
:CONTrol:DSIM[1]2|3|4[:EXTernal]:PORT:CONFig SERial|PARallel
:CONTrol:DSIM[1]2|3|4[:EXTernal]:PORT:CONFig?
This command selects the data transmission type used for communication between the N5102A module and the device under test. This selection affects the clock and sample rate ranges.
:CONTrol:DSIM[1]2|3|4[:EXTernal]:PORT:PMAPping IQ2IQ|IQ2IQI|IQ2IIQ
:CONTrol:DSIM[1]2|3|4[:EXTernal]:PORT:PMAPping?
This choice selects the port mapping type for parallel transmission only.
|
IQ2IQ |
With this choice, samples are transmitted as 16 bits of ’I’ followed by 16 bits of ’Q’; a complete sample is 32 bits or 4 bytes. At the device interface, the 16 bits of ’I’ are on the 16 ’I’ parallel lines; the 16 bits of ’Q’ are on the 16 ’Q’ parallel lines. |
|
IQ2IQI |
With this choice, samples are transmitted as 16 bits of ’I’ followed by 16 bits of ’Q’; a complete sample is 32 bits or 4 bytes. At the device interface, the 16 bits of ’I’ and the 16 bits of ’Q’ are both on the 16 ’I’ parallel lines. The ’I’ and ’Q’ bits are interleaved, with the ’Q’ bits coinciding with the rising edge of the clock, and the ’I’ bits occurring with the falling edge of the clock. The ’Q’ bits for a given sample precede the ’I’ bits for that sample. |
|
IQ2IIQ |
With this choice, samples are transmitted as 16 bits of ’I’ followed by 16 bits of ’Q’; a complete sample is 32 bits or 4 bytes. At the device interface, the 16 bits of ’I’ and the 16 bits of ’Q’ are both on the 16 ’I’ parallel lines. The ’I’ and ’Q’ bits are interleaved, with the ’I’ bits coinciding with the rising edge of the clock, and the ’Q’ bits occurring with the falling edge of the clock. The ’I’ bits for a given sample precede the ’Q’ bits for that sample. |
:CONTrol:DSIM[1]2|3|4[:EXTernal]:PORT:SMAPping IQ2IQ|IQ2SIIQ|IQ2BIIQ
:CONTrol:DSIM[1]2|3|4[:EXTernal]:PORT:SMAPping?
This command selects the port mapping type for serial transmission only.
|
IQ2IQ |
With this choice, samples are transmitted as 16 bits of ’I’ followed by 16 bits of ’Q’; a complete sample is 32 bits or 4 bytes. At the device interface, the 16 ’I’ bits of a sample appear as a serial stream on the I0 line. The 16 ’Q’ bits of a sample appear on the I1 line. Accompanying these two data lines are separate lines for clock and frame signals. The frame signal goes high for one clock cycle during I0 and Q0; for the rest of the sample, the frame is low. |
|
|
|
||
|
IQ2SIIQ |
With this choice, samples are transmitted as 16 bits of ’I’ followed by 16 bits of ’Q’; a complete sample is 32 bits or 4 bytes. At the device interface, the 16 'I’ bits as well as the 16 ’Q’ bits of a sample appear as a single serial stream on the I0 line. The ’I’ bits of a given sample precede the associated 16 ’Q’ bits. The frame signal goes high for one clock cycle during the first ’I’ bit of a sample; for the rest of the sample, the frame signal is low. |
|
|
|
||
|
IQ2BIIQ |
With this choice, samples are transmitted as 16 bits of ’I’ followed by 16 bits of ’Q’; a complete sample is 32 bits or 4 bytes. At the device interface, the 16 ’I’ bits as well as the 16 ’Q’ bits of a sample appear as a single serial stream on the I0 line, with each 'I’ bit preceding the associated ’Q’ bit. The frame signal goes high for one clock cycle during the first ’I’ bit of a sample; during the rest of the sample, the frame signal is low. |
|
|
|
||