These commands set the input parameters when using external-in configurations.
[:SOURce]:IO[1]|2|3|4|5|6|7|8:INPut:LSTate HLValue|ZERO
[:SOURce]:RADio[1]2|3|4:ARB:INPut:LSTate?
This command sets the state that the output holds when the waveform playing stops.
|
HLValue |
This choice holds the last I and Q sample value on the input until the next waveform is played. |
|
ZERO |
This choice sets the input value to zero. |
:CONTrol:IO[1]|2|3|4|5|6|7|8:INPut:RSCaling <val>
:CONTrol:IO[1]|2|3|4|5|6|7|8:INPut:RSCaling?
This command adjusts the scaling value for the input waveform.
The variable <val> is expressed in dB.
Range: – 60 to 0