These commands are used for memory storage and retrieval.
|
|
:MEMory:DATA and :MEMory:APPend commands are provided for backward compatibility with previous instruments. |
:MMEMory:DATA "<file_name>",#ABC or
:MEMory:DATA "<file_name>",#ABC
This command writes <data> into "<file_name>", where <data> is in 488.2 block format.
The PXB expects to see waveform data as block data (binary files). The IEEE standard 488.2-1992 section 7.7.6 defines block data. The following example shows how to structure a SCPI command for downloading waveform data where #ABC represents the block data.
|
"<file_name>" |
The file name can be the short name, full file path, or NVWFM format.
|
|
# |
This character indicates the beginning of the data block. |
|
A |
Number of decimal digits present in B |
|
B |
Decimal number specifying the number of data bytes to follow in C |
|
C |
Actual binary waveform data |
:MMEMory:DATA:APPend "<file_name>",<blockdata>
or
:MEMory:DATA:APPend "<file_name>",<blockdata>
This command appends byte data to an existing file stored in memory in the specified "<file name>".
|
"<file_name>" |
This variable names the destination file. |
|
<blockdata> |
This parameter represents the file length and data to be appended. |
Example: "NVWFM1:IQ_Data",#14Y9oL
|
"NVWFM1:IQ_Data" |
File path and file name. (D:\Waveforms\Channel1 is implied by reference.) |
|
#149oL |
Data block |
|
# |
This character indicates the beginning of the data block. |
|
1 |
Number of digits in the byte count. |
|
4 |
Byte count |
|
Y9oL |
Four byes of data to be appended (used for example purpose only) |
|
|
The following commands are not supported for non-volatile waveform memory (NVWFM). |
:MMEMory:CATalog? "<file_system>"
This query outputs a list of the files from the specified file system. The return data will be in the following form: <mem_used>,<mem_free>{,"<file_listing>"}.
:MMEMory:CDIRectory "[<directory_name>]", "[<directory_name>]"
:MMEMory:CDIRectory?
This command changes the directory name for a file system. If no parameter is specified, the directory is set to the *RST value. At *RST, this value is set to the default user data directory. The query returns the full path of the default directory.
:MMEMory:COPY "<file_name>","<file_name>"
This command makes a duplicate of the requested file.
:MMEMory:DELete "<file_name>",<directory_name>
This command removes a file from the specified directory.
:MMEMory:MDIRectory <directory_name>
This command creates a new directory where the <directory
name> parameter specifies the name of the new directory.
:MMEMory:MOVE "<src_file>","<src_file_1>"
This command renames the src_file to src_file_1.
:MMEMory:RDIRectory <directory_name>
This command removes a directory where the <directory_name>
parameter specifies the name of the directory to be removed. All files
and directories under the specified directory are also removed.