Quick Start Guide (N5105-90004)
Firmware Upgrade Guide (N5105-90013)
Security Features (N5105-90014)
MIMO Channel Modeling and Emulation Test Challenges Application Note (5989-8973EN)
8960 Remote Operation/Automation with Vee Example
8960-PXB HSDPA Dual-Channel Baseband Fading Test Procedure
8960-PXB HSDPA MIMO Baseband Fading Test Procedure
|
|
You must have the VISA COM library (part of the Agilent IO Libraries Suite) and Visual Studio 2005 installed to build and run these programming examples. The Agilent IO Libraries Suite includes help for the various versions of VISA/SICL drivers. There are also programming examples that show how to use these drivers with the various programming languages. |