Selecting Quick Setups in the tree view displays a list of quick setups to help you begin signal capture or playback using a previously saved configuration.
You can use the System Configuration Wizard to start a new setup using actual hardware, or you can choose from three predefined simulated hardware setups. You can then customize the settings and save as a quick setup for later use.
The predefined quick setups enable you to test the setup parameters in simulated hardware mode. You can modify a setup as needed and save the modified file using the Save as Quick Setup button. You cannot delete the predefined quick setups.
The following predefined simulated hardware quick setups are available:
RF Playback
Digital Playback
Capture
|
|
There are no predefined quick setups for actual hardware connections. If you are using actual hardware (N5101A PCI card to N5102A module or ESG/PSG), you need to establish a hardware connection using the System Configuration Wizard before saving as a quick setup. |
Whether you configured your setup to use simulated or actual hardware, you can save it as a quick setup. Use the following buttons to manage your quick setups:
Click this button to save the current software configuration as a custom quick setup. A window appears, enabling you to enter a label for the quick setup.
Click this button to delete a custom quick setup icon from the quick setup view. A window appears, enabling you to choose the quick setup you want to delete.

Click this button to rename a custom quick setup. A window appears enabling you to choose and rename the quick setup.