|
|
Features depend on installed hardware and firmware options in the E4438C ESG and E8267D PSG vector signal generators. |
Bug Fixes:
Changed the default value of the Playback ESG/PSG Signal Generator Frequency setting from 2.0 GHz to 1.0 GHz.
Bug Fixes:
Updated the software to allow installation of the N5110B Signal Studio for Capture and Playback application on a PC running Agilent IO Libraries Suite Version 15.0 or higher.
Bug Fixes:
Modified the hardware wizard DRAM test so that the new DRAM chips (N5110B-022) are recognized.
Bug Fixes:
Updated the software to correct playback so that once the waveform file is loaded into DRAM, the same waveform file will not be reloaded when Play is selected.
|
|
However, the waveform file will be reloaded if the file's time-date stamp is changed to a more recent value after it was loaded into DRAM. |
Bug Fixes:
Updated software to correct waveform streaming problems with file sizes larger than 128 MB.
|
|
The waveform file will reload if it is changed between waveform name selection (initial pre-buffering) and the start of waveform playback. |
Enhancements:
Supports dual instances of N5110B software for waveform playback from DRAM of second N5101A-022 PCI card.
Supports synchronized start of waveform playback between instances via hardware trigger input to both N5101A PCI cards.
Bug Fixes:
Corrected a problem with loading waveforms specified in the settings and quick setup files.
Memory usage changed to release more PC memory when no longer in use.
LabVIEW
Enhancements:
Updated the help system to include detailed information on PC workstation requirements for HDD playback.
Updated help system to include installation information, release notes, and technical overview.
Software version 1.0.52.0 is the initial release of the N5110B Baseband Studio for Waveform Capture and Playback software.
Capture or playback digital IQ/IF signals up to 200/400 MSa/s
Use the 2 GB memory (512 MSa) to playback long time records of unique test scenarios
Playback custom I/Q waveform files to generate digital IQ, analog IQ or RF test stimuli
Connect with the digital signal interface module to communicate with your baseband subsystem
Connect with the 89600 Series VSA software for online or post-processing of captured data
Connect with the E4438C ESG or E8267D PSG to up-convert signals to RF or microwave frequencies
Comprehensive user interface provides essential control of the software, hardware, and operations in one place
Use tools such as markers and triggers to stimulate your device