5G NR
Adds a new component carrier into waveform. Up to 512 component carriers can be used. The valid index range is from 0 to the component carrier count minus 1.
|
GUI Location |
Apps > 5G NR > Carrier > + sign to Add |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier:ADD DL|UL|PRACh|CW |
|
SCPI Example |
RAD:NR5G:WAV:CCAR:ADD UL |
Deletes the specified carrier and its associated settings. A re-Index of the remaining carriers is done.
|
GUI Location |
Apps > 5G NR > Carrier > Ellipsis icon > Delete |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier:DELete <integer> |
|
SCPI Example |
RAD:NR5G:WAV:CCAR:DEL 0 |
Copies the currently selected carrier to the last column of the setup table. The maximum number is 32.
|
GUI Location |
Apps > 5G NR > Carrier > Ellipsis icon > Copy |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier:COPY <integer> |
|
SCPI Example |
RAD:NR5G:WAV:CCAR:COPY 0 |
Displays or returns the number of component carriers.
|
GUI Location |
Apps > 5G NR > Carrier > displays the configured carriers |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier:COUNt? |
|
SCPI Example |
RAD:NR5G:WAV:CCAR:COUN? |
| Preset | 1 |
|
State Saved |
No |
Sets the number of antennas for each generation. It is used for MIMO configuration. The "Antenna Port(s) Generated" parameter in the Channel Setup node for DL-SCH, UL-SCH, CSI-RS, and SRS allows you to configure the mapping between antenna and logical antenna port.
|
GUI Location |
Apps > 5G NR > Waveform > Basic > Total Number of Antennas |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:ANTenna:COUNt <integer> [:SOURce]:RADio:NR5G:WAVeform:ANTenna:COUNt? |
|
SCPI Example |
RAD:NR5G:WAV:ANT:COUN 2 RAD:NR5G:WAV:ANT:COUN? |
|
Couplings |
When Capability is set to RTIMe, the maximum value allowed for "Total Number of Antennas" is 2. |
|
Preset |
1 |
|
State Saved |
Yes |
|
Min |
1 |
|
Max |
24 The Max value for Real-time uplink is 2. |
|
GUI Location |
Apps > 5G NR > Waveform > Basic > Required License Version Date |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:LVERsion:DATE:REQuired? |
|
SCPI Example |
|
|
Preset |
2021.0801 |
|
State Saved |
Yes |
Enter the comment for the waveform, up to 32 characters.
|
GUI Location |
Apps > 5G NR > Waveform > Basic > Waveform Comment |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:COMMent <string> [:SOURce]:RADio:NR5G:WAVeform:COMMent? |
|
SCPI Example |
|
|
Couplings |
The max length of waveform Comment is 32 . The inputted string will be truncated from tail if the length is greater than 32. |
|
Preset |
"" |
|
State Saved |
Yes |
Displays the supported version of 3GPP specifications:
Default (fixed): V17.4.0 (2022-12)
This read-only field displays the supported version of 3GPP specifications:
TS 38.211 Physical Channels and Modulation
TS 38.212 Multiplexing and Channel Coding
TS 38.213 Physical Layer Procedures for Control
TS 38.214 Physical Layer Procedures for Data
|
GUI Location |
Apps > 5G NR > Waveform > Basic > 3GPP Version |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:TGPP:VERSion? |
|
SCPI Example |
RAD:NR5G:WAV:TGPP:VERS? |
|
Preset |
V17.4.0 (2022-12) |
|
State Saved |
No |
Allows you to specify a sample rate of your choice.
Entering *n automatically multiplies the current sample rate by that number. For example, entering *3 sets 368.64 Msa/s automatically. You can also enter fractional numbers, for example, *1.2.
|
GUI Location |
Apps > 5G NR > Waveform > Basic > User Defined Sample Rate |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:SRATe:USER[:STATe] ON|OFF|1|0 [:SOURce]:RADio:NR5G:WAVeform:SRATe:USER[:STATe]? |
|
SCPI Example |
|
|
Preset |
Off |
|
State Saved |
Yes |
Displays or returns the sample rate, which is automatically calculated to meet the requirement of waveform settings and connected instrument.
If User Defined Sample Rate is disabled, the sample rate is automatically calculated to meet the requirement of the waveform settings and connected instrument, otherwise this value can be editable to input a user-defined sample rate.
If the connected instrument is M8190A Direct mode, the auto calculated sample rate is larger than 125 MHz to meet the instrument limitation.
If the connected instrument is M8190A DUC mode, the sample rate is auto calculated based on the interpolated mode to meet the instrument limitation.
|
GUI Location |
Apps > 5G NR > Waveform > Basic > Sample Rate |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:SRATe? |
|
SCPI Example |
RAD:NR5G:WAV:SRAT? |
|
Preset |
122.88 MHz |
|
State Saved |
Yes |
|
Min |
7.68 MHz |
|
Max |
12 GHz |
|
Resolution |
1 Hz |
Range: 0.001 to 1000
Default: 1
Set the Time Scale Factor of the sample rate.
When Phase Compensation is set to Auto (Real-time) or Manual (Real-time) this parameter is read-only and set to 1.
|
GUI Location |
Apps > 5G NR > Waveform > Basic > Time Scale Factor |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:TSFactor <real> [:SOURce]:RADio:NR5G:WAVeform:TSFactor? |
|
SCPI Example |
|
|
Preset |
1 |
|
State Saved |
Yes |
Defines the number of radio frames included in the waveform.
If the carrier is a downlink carrier and SSB is enabled, you need to change this parameter to match the SSB period, otherwise a warning is generated.
When the Number of Radio Frames is not 1, different configurations for different frames are supported. For SS/PBCH, the multi-frame configuration is determined by the SSB period. For other channels, edit the Allocated Slots field to set multi-frame configuration.
|
GUI Location |
Apps > 5G NR > Waveform > Basic > Number of Radio Frames |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:FRAMes:COUNt <integer> [:SOURce]:RADio:NR5G:WAVeform:FRAMes:COUNt? |
|
SCPI Example |
RAD:NR5G:WAV:FRAM:COUN 2 RAD:NR5G:WAV:FRAM:COUN? |
|
Notes |
The max value is determined by the total waveform length which should be less than 2G samples. |
|
Preset |
1 |
|
State Saved |
Yes |
|
Min |
1 |
|
Max |
1627 |
|
Resolution |
1 |
|
GUI Location |
Apps > 5G NR > Waveform > Basic > Subframe Offset |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:SFRame:OFFSet <integer> [:SOURce]:RADio:NR5G:WAVeform:SFRame:OFFSet? |
|
SCPI Example |
|
|
Preset |
0 |
|
State Saved |
Yes |
|
Min |
1 |
|
Max |
9 |
Sets the number of subframes to generate partial radio frame when the Number of Radio Frames is 1.
|
GUI Location |
Apps > 5G NR > Waveform > Basic > Number of Subframes |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:SFRame:NUMBer <integer> [:SOURce]:RADio:NR5G:WAVeform:SFRame:NUMBer? |
|
SCPI Example |
|
| Couplings | Max = 10 - Subframe Offset |
|
Preset |
10 |
|
State Saved |
Yes |
|
Min |
1 |
Sets the slot offset in the subframe to generate partial subframe, when the number of subframes is 1. This parameter is only applicable for a single downlink/uplink carrier and single numerology case.
The range is based on the numerology of the carrier.
|
GUI Location |
Apps > 5G NR > Waveform > Basic > Slot Offset in Subframes |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:SFRame:SLOT:OFFSet <integer> [:SOURce]:RADio:NR5G:WAVeform:SFRame:SLOT:OFFSet? |
|
SCPI Example |
|
|
Preset |
1 |
|
State Saved |
Yes |
|
Min |
-1 |
Sets the number of slots in the subframe to generate a partial subframe, when the number of subframe is 1. This parameter is only applicable for single downlink/uplink carrier and single numerology case.
The range is based on the numerology of the carrier.
|
GUI Location |
Apps > 5G NR > Waveform > Basic > Number of Slots in Subframes |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:SFRame:SLOT:NUMBer <integer> [:SOURce]:RADio:NR5G:WAVeform:SFRame:SLOT:NUMBer? |
|
SCPI Example |
|
|
Preset |
-1 |
|
State Saved |
Yes |
|
Min |
-1 |
Sets or displays the number of sample points in the waveform. This value can be edit if there is no carrier in the waveform, otherwise it is read-only and will be automatically updated with waveform setting changes.
|
GUI Location |
Apps > 5G NR > Waveform > Basic > Total Sample Points |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:SAMPles:COUNt? |
|
SCPI Example |
RAD:NR5G:WAV:SAMP:COUN? |
|
Preset |
1228800 |
|
State Saved |
No |
Displays the waveform length in seconds. This value is read-only and will be automatically updated when waveform settings are changed.
|
GUI Location |
Apps > 5G NR > Waveform > Basic > Waveform Length |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:LENGth? |
|
SCPI Example |
RAD:NR5G:WAV:LENG? |
|
Preset |
10 ms |
|
State Saved |
No |
Enables or disables the mirror spectrum for the waveform. If enabled, I and Q data of the waveform are swapped to make the mirror spectrum.
|
GUI Location |
Apps > 5G NR > Waveform > Basic > Mirror Spectrum |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:MIRRor:SPECtrum[:STATe] ON|OFF|1|0 [:SOURce]:RADio:NR5G:WAVeform:MIRRor:SPECtrum[:STATe]? |
|
SCPI Example |
RAD:NR5G:WAV:MIRR:SPEC OFF RAD:NR5G:WAV:MIRR:SPEC? |
|
Preset |
OFF |
|
State Saved |
Yes |
|
Range |
On | Off |
Specifies the phase compensation mode on the baseband signal before performing an up conversion.
|
GUI Location |
Apps > 5G NR > Waveform > Basic > Phase Compensation |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:PHASe:COMPensation AUTO|MANual|OFF [:SOURce]:RADio:NR5G:WAVeform:PHASe:COMPensation? |
|
SCPI Example |
RAD:NR5G:WAV:PHAS:COMP MAN RAD:NR5G:WAV:PHAS:COMP? |
|
Couplings |
If set to AUTO, the RF Frequency is used , and RF Frequency is coupled with the frequency of instrument. If set to manual, the RF Frequency is used and RF Frequency can be set. If set to off, phase compensation is disabled. |
|
Preset |
Auto |
|
State Saved |
Yes |
Controls the radio frequency when phase compensation is applied on a baseband signal. It is automatically coupled with the frequency of instrument when Phase Compensation is set to Auto, and can be edited when Phase Compensation is set to Manual, but not visible when Phase Compensation is Off.
|
GUI Location |
Apps > 5G NR > Waveform > Basic > Radio Frequency |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:PHASe:COMPensation:FREQuency <freq> [:SOURce]:RADio:NR5G:WAVeform:PHASe:COMPensation:FREQuency? [MAXimum|MINimum] |
|
SCPI Example |
RAD:NR5G:WAV:PHAS:COMP:FREQ 100MHz RAD:NR5G:WAV:PHAS:COMP:FREQ? |
|
Preset |
1 GHz |
|
State Saved |
Yes |
|
Min |
0 |
|
Max |
100 GHz |
|
Resolution |
1 Hz |
Selects the source for marker 1.
Waveform Start indicates the beginning of the waveform.
Frame Start indicates the beginning of each frame in the waveform.
RF Blanking Control indicates the burst part in the waveform.
RF ALC Control indicates the part used for ALC control in the waveform.
|
GUI Location |
Apps > 5G NR > Waveform > Marker > Marker 1 Source |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:M1Source WSTart|FSTart|BLANking|ALC [:SOURce]:RADio:NR5G:WAVeform:M1Source? |
|
SCPI Example |
RAD:NR5G:WAV:M1S FST RAD:NR5G:WAV:M1S? |
|
Preset |
Wavefrom Start (WSTart) |
|
State Saved |
Yes |
Selects the source for marker 2.
Waveform Start indicates the beginning of the waveform.
Frame Start indicates the beginning of each frame in the waveform.
RF Blanking Control indicates the burst part in the waveform.
RF ALC Control indicates the part used for ALC control in the waveform.
|
GUI Location |
Apps > 5G NR > Waveform > Marker > Marker 2 Source |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:M2Source WSTart|FSTart|BLANking|ALC [:SOURce]:RADio:NR5G:WAVeform:M2Source? |
|
SCPI Example |
RAD:NR5G:WAV:M2S FST RAD:NR5G:WAV:M2S? |
|
Preset |
Frame Start (FSTart) |
|
State Saved |
Yes |
Displays or returns the source for marker 3. RF Blanking Control is always used as Marker 3 source.
|
GUI Location |
Apps > 5G NR > Waveform > Marker > Marker 3 Source |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:M3Source? |
|
SCPI Example |
RAD:NR5G:WAV:M3S? |
|
Preset |
Blanking |
|
State Saved |
Yes |
Displays or returns the source for marker 4. RF ALC Control is always used as the Marker 4 source.
|
GUI Location |
Apps > 5G NR > Waveform > Marker > Marker 4 Source |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:M4Source? |
|
SCPI Example |
RAD:NR5G:WAV:M4S? |
| Preset | ALC |
|
State Saved |
Yes |
|
GUI Location |
Apps > 5G NR > Waveform > Crest Factor Reduction > Crest Factor Reduction |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:CFReduction[:STATe] ON|OFF|1|0 [:SOURce]:RADio:NR5G:WAVeform:CFReduction[:STATe]? |
|
SCPI Example |
|
| Preset | Off |
|
State Saved |
Yes |
To view this function, Crest Factor Reduction must be enabled.
Sets the peak-to-average power ratio (PAPR) value to achieve after crest factor reduction.
|
GUI Location |
Apps > 5G NR > Waveform > Crest Factor Reduction > Target PAPR |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:CFReduction:PAPR <real> [:SOURce]:RADio:NR5G:WAVeform:CFReduction:PAPR? |
|
SCPI Example |
|
| Preset | 8 |
|
State Saved |
Yes |
|
Min |
3 |
|
Max |
100 |
To view this function, Crest Factor Reduction must be enabled.
Specifies the maximum times of iteration. As iteration is increased, the PAPR value should converge to a steady level.
|
GUI Location |
Apps > 5G NR > Waveform > Crest Factor Reduction > Max Iteration |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:CFReduction:MITeration <integer> [:SOURce]:RADio:NR5G:WAVeform:CFReduction:MITeration? |
|
SCPI Example |
|
| Preset | 10 |
|
State Saved |
Yes |
|
Min |
1 |
|
Max |
100 |
To view this function, Crest Factor Reduction must be enabled.
Specifies the percentage of the cancellation pulses that can be removed.
|
GUI Location |
Apps > 5G NR > Waveform > Crest Factor Reduction > Canceling Percentage |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:CFReduction:CPERcent <real> [:SOURce]:RADio:NR5G:WAVeform:CFReduction:CPERcent? |
|
SCPI Example |
|
| Preset | 100 |
|
State Saved |
Yes |
|
Min |
0 |
|
Max |
100 |
To view this function, Crest Factor Reduction must be enabled.
A block is the range where a single cancellation pulse can be identified. If the waveform length is L, and the block size is B, then the number of blocks is N=floor(L/B)+1. Therefore, there will be N pulses at most to be removed.
|
GUI Location |
Apps > 5G NR > Waveform > Crest Factor Reduction > Block Size |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:CFReduction:BSIZe <integer> [:SOURce]:RADio:NR5G:WAVeform:CFReduction:BSIZe? |
|
SCPI Example |
|
| Preset | 1000 |
|
State Saved |
Yes |
|
Min |
20 |
To view this function, Crest Factor Reduction must be enabled.
Enter a string to set the filter mask to define a filter response in the frequency domain, separated by semicolon for each comma-separated frequency point/amplitude pair. When generating this filter mask, the frequency points between the specified points are linearly interpolated. When the carrier number or carrier frequency offset in the waveform is changed, this table will be automatically updated. You may need to adjust the mask manually to fit the actual signal bandwidth.
|
GUI Location |
Apps > 5G NR > Waveform > Crest Factor Reduction > Filter Mask |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:CFReduction:FMASk <string> [:SOURce]:RADio:NR5G:WAVeform:CFReduction:FMASk? |
|
SCPI Example |
|
| Preset | -60,-100;-50,0;50,0;60,-100 |
|
State Saved |
Yes |
Enables or disables additive white Gaussian noise (AWGN) in the waveform. When enabled, more parameters appear below.
|
GUI Location |
Apps > 5G NR > Waveform > AWGN > Enabled |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:AWGN:ARB[:STATe] ON|OFF|1|0 [:SOURce]:RADio:NR5G:WAVeform:AWGN:ARB[:STATe]? |
|
SCPI Example |
|
| Preset | Off |
|
State Saved |
Yes |
To view this function, AWGN must be enabled.
Sets the carrier to noise ratio. The carrier is at 0 dB .
|
GUI Location |
Apps > 5G NR > Waveform > AWGN > Carrier to Noise Ratio |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:AWGN:ARB:CNRatio <real> [:SOURce]:RADio:NR5G:WAVeform:AWGN:ARB:CNRatio? |
|
SCPI Example |
|
| Preset | 0 |
|
State Saved |
Yes |
|
Min |
-100 |
|
Max |
100 |
To view this function, AWGN must be enabled.
Sets the waveform bandwidth, it is automatically updated when parameters are related to frequency domain location changes.
|
GUI Location |
Apps > 5G NR > Waveform > AWGN > Carrier Bandwidth |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:AWGN:ARB:CBWIdth <real> [:SOURce]:RADio:NR5G:WAVeform:AWGN:ARB:CBWIdth? |
|
SCPI Example |
|
| Preset | 98280000 |
|
State Saved |
Yes |
To view this function, AWGN must be enabled.
Sets the noise bandwidth.
|
GUI Location |
Apps > 5G NR > Waveform > AWGN > Flat Noise Bandwidth |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:AWGN:ARB:FNBWidth <real> [:SOURce]:RADio:NR5G:WAVeform:AWGN:ARB:FNBWidth? |
|
SCPI Example |
|
| Preset | 98280000 |
|
State Saved |
Yes |
To view this function, AWGN must be enabled and the component carrier must be disabled. See Carrier General > Enabled.
Display the flat noise power offset compared to the signal generator power.
|
GUI Location |
Apps > 5G NR > Waveform > AWGN > Flat Noise Power Offset |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:AWGN:ARB:FNPoffset? |
|
SCPI Example |
|
| Preset | -0.969100130080564 |
|
State Saved |
Yes |
To view this function, AWGN must be enabled.
Displays the carrier power offset compare to the signal generator power.
|
GUI Location |
Apps > 5G NR > Waveform > AWGN > Carrier Power Offset |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:AWGN:ARB:CPOFfset? |
|
SCPI Example |
|
| Preset | -3.52182518111362 |
|
State Saved |
Yes |
Group and Signal settings determine where the specific antenna’s 5G waveform is played. Each antenna has its own group and signal settings. The maximum count of antennas is 8. When only one waveform is generated with Total Number of Antennas set to 1, the waveform file name will have a _G#S# suffix (
view image), based on the routing configuration, so you can specify different group/signal configurations to generate and playback the waveform.
Note that the following corner cases do not work ideally:
Case 1 for multiple antennas/waveforms configuration (i.e. Total Number of Antennas is > 1): If you route the same antenna’s waveform to a different signal of same group, the waveform played is not the latest generated one, but the first-generated waveform file because firmware does not support uploading waveform with same name multiple times in the group.
Case 2 for multiple antennas/waveforms configuration: If you route a different antenna’s waveform to same signal and same group, the waveform of antenna with biggest cardinality will be played. For example, if antenna 0 is routed to group 1 + signal 1, and antenna 1 is also routed to group 1 + signal 1, waveform of antenna 1 will be played.
Case 3: If you route waveform to a non-existing group and signal, no error will be prompted. But waveform will be played on the group with biggest suffix. For example, if you route waveform to group 4 + signal 7 while group 4 does not exist and current group count is 2, then 5G waveform will be played on group 2 + signal 7 (with 8-signals feature) or group 2 + signal 1 (without 8-signals feature).
|
GUI Location |
Apps > 5G NR > Waveform > Routing > Group |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:ROUTing{0:7}:GROup <integer> [:SOURce]:RADio:NR5G:WAVeform:ROUTing{0:7}:GROup? |
|
SCPI Example |
RAD:NR5G:WAV:ROUT:GRO 2 RAD:NR5G:WAV:ROUT:GRO? |
| Couplings |
How many routings can be defined is coupled with Total Number of Antennas. It means when Total Number of Antennas is 1, only one routing can be defined. If Total Number of Antennas is changed, Group will be coupled the cardinality of routing/Antenna + 1. For example, if Group is set to 2 of antenna 0, and then set Total Number of Antennas to 2, Group of antenna 0 will be coupled to 1 and Group of antenna 1 will be coupled to 2 automatically. |
| Preset |
1 |
|
State Saved |
Yes |
|
Min |
1 |
|
Max |
8 |
|
State Saved |
Yes |
|
GUI Location |
Apps > 5G NR > Waveform > Routing > Signal |
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform:ROUTing{0:7}:SIGNal <integer> [:SOURce]:RADio:NR5G:WAVeform:ROUTing{0:7}:SIGNal? |
|
SCPI Example |
RAD:NR5G:WAV:ROUT:SIGN 2 RAD:NR5G:WAV:ROUT:SIGN? |
| Couplings |
How many routings can be defined is coupled with Total Number of Antennas. It means when Total Number of Antennas is 1, only one routing can be defined. |
| Preset |
1 |
|
State Saved |
Yes |
|
Min |
1 |
|
Max |
8 |
|
State Saved |
Yes |
The graph view displays three different representations
of the generated waveform:
IQ,
Spectrum, and
CCDF.
Changes to the waveform configuration do not update the graph until you generate the waveform.
|
IQ |
Provides three different plots for viewing the I and Q waveforms: Power, I Plus Q, and I And Q |
|
Spectrum |
Displays the waveform spectrum (power vs. frequency). |
|
CCDF |
The CCDF graph displays the probability (in percentage) that the generated waveform's calculated peak-to-average power ratio (measured in dB) is greater than or equal to a specified level. The table to the left of the CCDF plot displays the calculated peak-to-average values for the current waveform. Reference - Select to view the reference curve. Acquire Reference - Sets the current waveform curve as the reference curve. Burst and Waveform toggle between the two settings Burst - Calculates the CCDF curve based on the generated I/Q waveform, excluding the off power period. Waveform - Calculates the CCDF curve based on entire generated I/Q waveform. |