Multi-Instrument

Required Option SNC

Overview

Prerequisites for Multi-Instrument Setup

Steps to Configure Multi-Instrument Setup

Step 1 - Configure Follower(s)

Make Cable Connections Between the Leader and Follower(s)

Select the Follower Mode

Step 2 - Configure Leader

Change the Mode to Leader

Add Followers

Apply Settings on Leader

Perform Alignment

GUI Settings and SCPI Commands for Multi-Instrument

Current Multi-Instrument Mode

Set Role and Reboot

Set Role and Power Down

Add Follower

Follower Count

Reboot All Instruments

Overview

You can use the multi-instrument feature to set up a system of multiple signal generator instruments that are cabled together enabling all channels of the system to be coherent in phase and trigger synchronously.

You need to configure one of the participating instruments in a multi-instrument setup as the leader and all other participating instruments as followers. Also, the multi-instrument setup requires cabling between the leader and follower(s).

The order in which you make the physical cabling between the participating instruments of the multi-instrument setup determines the order in which you need to add followers to the leader's configuration in the Multi-Instrument screen.

Prerequisites for Multi-Instrument Setup

Before updating firmware on leader/follower, ensure that the KDMI cable between the leader and follower is disconnected. If you start the firmware update with this cable connected, the firmware update will fail.

Steps to Configure Multi-Instrument Setup

Step 1 - Configure Follower(s)

Make Cable Connections Between the Leader and Follower(s)

Select the Follower Mode

Step 2 - Configure Leader

Step 1 - Configure Follower(s)

Always begin with setting up follower(s) in your multi-instrument setup.

On each follower instrument:

  1. Access the Configure Launch screen.

  2. Select the Multi-Instrument tab.
    Notice that by default, the Multi-Instrument Mode of an instrument is set to Standalone.

Make Cable Connections Between the Leader and Follower(s)

Select the Follower Mode

After the cabling is complete, select the Multi-Instrument Mode as Follower and then click OK on the message box to restart the signal generator application in the Follower mode.

Complete this step for all followers in your setup.

On clicking OK, the application begins the reboot process and then waits for the leader to be configured. The reboot screen displays the follower’s hostname and IP address and an indicator showing the follower is waiting. The follower instrument will wait as long as it takes for the leader to be configured. At any time, you can press Abort which will return the follower instrument to the Standalone mode.

You need to select the Follower mode only when you are switching an instrument from Standalone to Follower, or from Leader to Follower and you are rearranging the order of instruments in your multi-instrument setup. If you subsequently reboot the instrument, it will retain the set multi-mode configuration.
You cannot use an instrument cabled as a follower in the Standalone mode. An instrument that was previously a follower must have its cables returned to the original condition to operate in Standalone.

Step 2 - Configure Leader

When the cabling is in place and all followers have been launched in the Follower mode and are waiting for the leader, configure the following settings on the leader instrument.

Change the Mode to Leader

  1. Access the Configure Launch screen.

  2. Select the Multi-Instrument tab.

  3. Click the Leader option to configure the instrument as the leader.

Add Followers

On clicking the Leader option, the following screen is displayed. Use this screen to add followers.

  1. In the Follower table, specify the IP Address of the first Follower in your multi-instrument system.

  2. If there are more than one Follower, press the Add Follower button and repeat steps 1 and 2 until all Followers have been added.

The order in which you add Followers to this table must match the cabling order used for Followers.

If needed, use the Move Up and Move Down buttons to change the ordering of the entries in the table.

Apply Settings on Leader

After completing the required configuration settings on leader, press Apply to apply the leader settings in your multi-instrument setup.

On pressing Apply:

Perform Alignment

After the instruments have been successfully launched and configured as leader and follower(s), perform the alignment.

Before running the alignment, make sure RF is off and no signals are enabled so that the alignment process is not impacted.

On the leader:

  1. Access the Sync menu using the Status icon in the top bar.

  2. In the Status Viewer, navigate to the Synchronization page using the SYNC indicator.

  3. Press the Clear Alignment button and then the Perform Alignment button.

This operation will take several minutes depending on the number of instruments in the multi-instrument system.

Once the alignment is performed, you need to redo the Clear Alignment and Perform Alignment only when:

When an instrument starts as a follower:
- its reference source is set to External, 10 MHz and cannot be changed.
- its global trigger source comes from the leader and cannot be changed.

Rebooting the Instruments After Initial Leader-Followers Configuration

Once the initial configuration of leader and follower(s) has been established, if the instruments are rebooted, the follower(s) will begin to boot and wait for the leader. The leader will begin to boot and then wait for the follower(s) to connect. While waiting, the leader will display a progress indicator, with the opportunity to Abort. On pressing Abort, the leader instrument starts in the Standalone mode.

Reconfiguring a Follower as Standalone or Leader

When an instrument has been cabled as a Follower and is to be reconfigured as Standalone or Leader, the cabling for the instrument must be returned to the original condition.

GUI Settings and SCPI Commands for Multi-Instrument

Current Multi-Instrument Mode

In a system of multiple signal generator instruments, each instrument must be configured for the role it plays in the physical connections of the system. You can set an instrument in one of the following three modes.

SCPI Command

SYSTem:SYNChronize:ROLE STANdalone|LEADer|FOLLower

SYSTem:SYNChronize:ROLE?

SCPI Example

SYST:SYNC:ROLE LEAD

SYST:SYNC:ROLE?

Notes

Attempting to change the value of this setting on instruments without Option SNC raises the error 703,"Feature not supported; Multi-Instrument requires Option SNC"

Preset

This is unaffected by a Preset but is set to STANDalone on a "Restore System Settings to Default Values."

Range Standalone|Leader|Follower

State Saved

Persistent, survives preset and power cycle but not saved in the instrument state.

Set Role and Reboot

Remote command only

Sets the multi-instrument synchronization role and immediately performs a cold reboot of the instrument so that the new role takes effect on the next boot.

Use this when the role change requires a full system reboot to apply.

There is no query form for the command.

SCPI Command

:SYSTem:SYNChronize:ROLE:REBoot STANdalone|LEADer|FOLLower

SCPI Example

SYST:SYNC:ROLE:REB FOLL

Sets the role to Follower and cold-reboots the instrument

Notes

This command sets the desired role and triggers an immediate cold reboot.

You cannot use *WAI or *OPC? to synchronize operation after the restart.

A remote program must wait until instrument shutdown completes before attempting to reconnect.

Attempting to use this command on instruments without option SNC raises the error 703,"Feature not supported; Multi-Instrument requires option SNC"

State Saved

No

Set Role and Power Down

Remote command only

Sets the multi-instrument synchronization role and then performs a normal system shutdown (power down).

The instrument must be manually powered back on, after which, it boots into the new role.

There is no query form for the command.

SCPI Command

:SYSTem:SYNChronize:ROLE:PDOWn STANdalone|LEADer|FOLLower

SCPI Example

SYST:SYNC:ROLE:PDOW LEAD

Sets the role to Leader and powers down the instrument.

Notes

Attempting to use this command on instruments without option SNC raises the error 703,"Feature not supported; Multi-Instrument requires option SNC"

State Saved

No

Add Follower

Configures the networking address and order of the Follower(s) on the Leader instrument. The order of the addresses for the followers much coincide with the physical cabling of the multiple instrument arrangement.

SCPI Command

SYSTem:SYNChronize:FOLLowers <string>,…

SYSTem:SYNChronize:FOLLowers?

SCPI Example

SYST:SYNC:FOLL "instrument2","192.168.0.100","instrument4"

SYST:SYNC:FOLL?

Notes

The supplied <string>,… is a string list. Each string is separated with a comma. The strings in the list is the IP Address or hostname of the instruments configured in a multi-instrument system.

The order of the entries in the list of followers must match the physical connections of the instruments in the system.

Attempting to change the value of this setting on instruments without Option SNC raises the error 703,"Feature not supported; Multi-Instrument requires Option SNC"

Preset This is unaffected by a Preset but is cleared on a "Restore System Settings to Default Values."

State Saved

Persistent, survives preset and power cycle but not saved in the instrument state.

Follower Count

Remote Command only.

Query only.

Returns the total number of followers configured for multi-instrument setup.

SCPI Command

SYSTem:SYNChronize:FOLLowers:COUNt?

SCPI Example

SYST:SYNC:FOLL:COUN?

State Saved

No

Reboot All Instruments

Only supported on the instrument designated as Leader in the multi-instrument setup

At times, changes to Configure Launch require rebooting all instruments participating in the multi-instrument setup. In such situations, this command is recommended to initiate the reboot for all participating instruments.

SCPI Command

:SYSTem:SYNChronize:REBoot

SCPI Example

:SYST:SYNC:REB

Executes a shutdown and reboot of all instruments in the multi-instrument arrangement.

Notes

You cannot use *WAI or *OPC? to synchronize operation after a restart. This command stops and restarts the instrument application, thus the SCPI operation is terminated and restarted. A remote program must wait until instrument shutdown completes before sending any connection request to avoid connecting to the shutting down instrument. It should then attempt a connection. Some connection methods such as GPIB might require repeated attempts until successful.