Reference

Reference ClosedSetup

Reference Source

Current Reference Source

Reference Source Auto

External Reference Frequency

External Reference Locking Range

Reference State

Reference Out

LF Out (100 MHz Out)

HF Out (19.2 GHz Out)

The Reference tab lets you configure the frequency reference for the instrument.

For Option 1ER, the user interface appears and behaves differently as shown in the sample screens below.

GUI Location

System Menu (triple bar icon) > Settings (gear icon) > Reference

Standard User Interface for Reference

Option 1ER User Interface for Reference

Reference Source

Sets the source for the frequency reference. Choices include the following:

The reference indicator field in the notifications bar at the bottom of the GUI displays the currently selected Reference Source and its current state.

When set to External, the frequency of the external signal can be specified with the External Reference Frequency setting.

If the external reference becomes unlocked or fails, after you correct the issue, toggle the Frequency Reference Source to Internal and back to External to update the Reference State status.

GUI Location

System Menu (triple bar icon) > Settings (gear icon) > Reference >Reference Source

SCPI Command

[:SOURce]:ROSCillator:SOURce INTernal|EXTernal

[:SOURce]:ROSCillator:SOURce?

SCPI Example

:ROSC:SOUR EXT

:ROSC:SOUR?

Notes

Changing the reference may take up to 30 seconds to regain frequency lock. For remote control operation, ensure your VISA timeout is set to 30 seconds (or more) when executing this command.

Range

Internal | External

Preset This is unaffected by a Preset but is set to INTernal on a "Restore System Settings to Default Values."
State Saved Persistent, survives preset and power cycle but not saved in the instrument state.
Backwards Compatibility SCPI

E82X7D, E8663D, N51xxB:

[:SOURce]:ROSCillator:SOURce

Backwards Compatibility Notes

For N51xxB:

SCPI query reports the setting’s stored value, not what is actively being applied to the hardware. This command differs from this prior behavior. To query what source is actively applied to hardware, see Current Reference Source setting.

Current Reference Source

Remote command only.

Returns the current reference source being applied to the instrument. Possible sources are:

See the Reference Source setting for more information.

SCPI Command

[:SOURce]:ROSCillator:SOURce:CURRent?

SCPI Example

:ROSC:SOUR:CURR?

  For SG6420A: - An external 2.4 GHz reference source cannot be detected automatically. The reference source auto setting should be turned off when using a 2.4 GHz external reference to prevent unitentionally locking to the wrong signal. The external reference frequency and external reference locking range settings have no effect when the source is set to external 2.4 GHz.
Range Internal|External|

Reference Source Auto

Enables or disables the ability of the signal generator to automatically switch between the Internal and External reference oscillator.

GUI Location

System Menu (triple bar icon) > Settings (gear icon) > Reference > Auto

SCPI Command

[:SOURce]:ROSCillator:SOURce:AUTO ON|OFF|1|0

[:SOURce]:ROSCillator:SOURce:AUTO?

SCPI Example

:ROSC:SOUR:AUTO ON

:ROSC:SOUR:AUTO?

Notes Changing the reference may take up to 30 seconds to regain frequency lock. For remote control operation, ensure your VISA timeout is set to 30 seconds (or more) when executing this command.
Preset This is unaffected by a Preset but is set to OFF on a "Restore System Settings to Default Values."
State Saved Persistent, survives preset and power cycle but not saved in the instrument state.

External Reference Frequency

Sets the external reference frequency.

After changing the External Reference Frequency, wait up to 30 seconds for the instrument’s frequency to settle.

GUI Location

System Menu (triple bar icon) > Settings (gear icon) > Reference > External Reference Frequency

SCPI Command

[:SOURce]:ROSCillator:FREQuency:EXTernal <freq>

[:SOURce]:ROSCillator:FREQuency:EXTernal?

SCPI Example

:ROSC:FREQ:EXT 100 MHZ

Preset

This is unaffected by a Preset but is set to 10 MHz on a "Restore System Settings to Default Values."

State Saved

Persistent, survives preset and power cycle but not saved in the instrument state.

Notes

Changing the reference frequency may take up to 30 seconds to regain frequency lock.  For remote control operation, ensure your VISA timeout is set to 30 seconds (or more) when executing this command.

For N5185A/N5186A with Option 1ER:

  • Valid input for <freq> can be from 1 MHz to 110 MHz.

For N5185A/N5186A without Option 1ER:

  • The only valid selection for <freq> is 10 MHz. Any other value will generate the error "703,Feature not supported; frequency value requires Option 1ER."

Min

Without Option 1ER: 10 MHz

With Option 1ER: 1 MHz

Max

For N5185A, N5186A

  • Without option 1ER: 10 MHz

  • With option 1ER: 110 MHZ

  • With option 1ER: 110 MHz

Resolution

With option 1ER: 0.1 Hz

Without option 1ER: Not applicable

External Reference Locking Range

The instrument provides two locking ranges for an externally supplied reference signal. Locking range set to Wide allows your reference signal to be further away in frequency from the selected value in External Reference Frequency, with a slight compromise in the phase noise performance of the instrument. Locking range set to Narrow provides the best phase noise on the instrument. See table below.

Locking Range

External Reference Requirements

Benefits

Wide

Within approximately +/- 1.0 ppm of the selected external reference frequency

Easier to lock to external reference

Narrow

Within approximately +/- 1.0 ppm of the selected external reference frequency

Better phase noise

GUI Location

System Menu (triple bar icon) > Settings (gear icon) > Reference > External Reference Locking Range

SCPI Command

[:SOURce]:ROSCillator:FREQuency:EXTernal:LRANge NARRow|WIDE

[:SOURce]:ROSCillator:FREQuency:EXTernal:LRANge?

SCPI Example

:ROSC:FREQ:EXT:LRAN WIDE

:ROSC:FREQ:EXT:LRAN?

Preset

This is unaffected by a Preset but is set to WIDE on a "Restore System Settings to Default Values."

State Saved

Persistent, survives preset and power cycle but not saved in the instrument state.

Backwards Compatibility SCPI

N51xxB:

[:SOURce]:ROSCillator:BANDwidth|BWIDth:EXTernal

Backwards Compatibility Notes

For N51xxB:

  • Alias [:SOURce]:ROSCillator:BANDwidth|BWIDth:EXTernal NARRow|WIDE to [:SOURce]:ROSCillator:FREQuency:EXTernal:LRANge NARRow|WIDE

  • Alias [:SOURce]:ROSCillator:BANDwidth|BWIDth:EXTernal MINimum to [:SOURce]:ROSCillator:FREQuency:EXTernal:LRANge NARRow

  • Alias [:SOURce]:ROSCillator:BANDwidth|BWIDth:EXTernal MAXimum to [:SOURce]:ROSCillator:FREQuency:EXTernal:LRANge WIDE

  • Alias [:SOURce]:ROSCillator:BANDwidth|BWIDth:EXTernal DEFault to [:SOURce]:ROSCillator:FREQuency:EXTernal:LRANge WIDE

  • When [:SOURce]:ROSCillator:BANDwidth|BWIDth:EXTernal <value> is sent and <value> is below 41.25 Hz, the External Reference Locking Range is set to NARRow.

  • When [:SOURce]:ROSCillator:BANDwidth|BWIDth:EXTernal <value> is sent and <value> is 41.25 Hz or above, the External Reference Locking Range is set to WIDE.

  • Query returns the current bandwidth in Hz: 9.5 for NARRow, 73.0 for WIDE

Reference State

Displays the current state of the frequency reference. The displayed state can help you understand whether the frequency reference is locked or if a failure occurred.

See Notifications Area for more information on various Reference states.

If the external reference becomes unlocked or fails, after you correct the issue, toggle the Frequency Reference Source to Internal and back to External to update the Reference State status.

Reference Out

The instrument, depending on model number, may contain several connectors that can be used for frequency references used by external test equipment or devices. Some of the connectors may be fixed outputs of frequency while others are switchable, or have selectable frequencies.

The Ref Out connector is controllable. The connector is normally on, providing a 10 MHz frequency reference by default. The connector can be switched off.

For N5185A/N5186A, the output frequency is selectable.

GUI Location

System Menu (triple bar icon) > Settings (gear icon) > Reference > Reference Out

SCPI Command

:ROUTe[:CONNectors]:REFerence:ROUTput OFF|F10|F100

:ROUTe[:CONNectors]:REFerence:ROUTput?

SCPI Example

ROUT:REF:ROUT OFF

Preset

This is unaffected by a Preset but is set to 10 MHz on a "Restore System Settings to Default Values."

Range OFF | 10 MHz | 100 MHz

State Saved

Persistent, survives preset and power cycle but not saved in the instrument state.

LF Out (100 MHz Out)

Remote command only

Provided to allow programmatic compatibility with other Keysight Technologies signal generators. Command is accepted but does nothing.

SCPI Command

:ROUTe[:CONNectors]:REFerence:LFOutput:STATe ON|OFF|1|0

:ROUTe[:CONNectors]:REFerence:LFOutput:STATe?

Notes Value is OFF and not changeable. Sending the SCPI command does not generate an error.

Preset

OFF

HF Out (19.2 GHz Out)

Remote command only

Provided to allow programmatic compatibility with other Keysight Technologies signal generators. Command is accepted but does nothing.

SCPI Command

:ROUTe[:CONNectors]:REFerence:HFOutput:STATe ON|OFF|1|0

:ROUTe[:CONNectors]:REFerence:HFOutput:STATe?

Notes Value is OFF and not changeable. Sending the SCPI command does not generate an error.

Preset

OFF