WLAN
|
SCPI Command |
[:SOURce]:RADio:WLAN:WAVeform:PHYSpec AC|AX|BE|BN [:SOURce]:RADio:WLAN:WAVeform:PHYSpec? |
|
SCPI Example |
|
|
Couplings |
|
|
Preset |
AX |
|
State Saved |
Yes |
Based on the PHY Specification that you selected in the Waveform > Basic tab, you can configure the waveform setup for the selected PHY specification.
If you select 802.11ac in the PHY Specification, then refer to the 802.11ac Waveform Settings topic to know about the waveform setup for 802.11ac.
If you select 802.11ax in the PHY Specification, then refer to the 802.11ax Waveform Settings topic to know about the waveform setup for 802.11ax.
If you select 802.11be in the PHY Specification, then refer to the 802.11be Waveform Settings topic to know about the waveform setup for 802.11be.
If you select 802.11bn in the PHY Specification, then refer to the 802.11bn Waveform Settings topic to know about the waveform setup for 802.11bn.
The Routing tab provides Group and Signal settings that determine where the specific waveform of WLAN is played. The waveform file name will have a _G#S# suffix based on the routing configuration. So, you can specify different Group/Signal to generate/playback/edit this waveform.
Assign the signal group number.
|
SCPI Command |
[:SOURce]:RADio:WLAN:WAVeform:ROUTing<channel>:GROup <integer> [:SOURce]:RADio:WLAN:WAVeform:ROUTing<channel>:GROup? |
|
SCPI Example |
|
|
Couplings |
|
|
Preset |
1 |
|
State Saved |
Yes |
|
Min |
1 |
|
Max |
8 |
Assign the signal number.
|
SCPI Command |
[:SOURce]:RADio:WLAN:WAVeform:ROUTing<channel>:SIGNal <integer> [:SOURce]:RADio:WLAN:WAVeform:ROUTing<channel>:SIGNal? |
|
SCPI Example |
|
|
Couplings |
|
|
Preset |
1 |
|
State Saved |
Yes |
|
Min |
1 |
|
Max |
8 |