Overview (Real-time)

The software supports the channels and reference signals as shown in Figure 1 below for an Uplink carrier compliant with the 3GPP standard release (March 2010). Refer to the Technical Overview for the 3GPP standard versions.

Figure 1. Supported channels and reference signals for HSPA Physical Layer

Supported Features

Description

Uplink/Downlink

Uplink only

Supported channels

DPCCH

DPDCH

  • DCHn

HS-DPCCH

HSUPA

  • E-DPCC

  • E-DPDCH

PRACH

  • RACH

Dynamically controlled parameters

HARQ ACK/NACK (external signal/user data)

Number of carriers

1 (single carrier per baseband section of the instrument)

Fast packet scheduling

Adaptive Modulation and Coding (AMC)

Provide "always on" connectivity testing

Continuous Packet Connectivity (CPC) with:

  • Discontinuous Reception (DRX)

  • Discontinuous Transmission (DTX)