To generate signals using the N7600B Signal Studio for W-CDMA/HSPA+ software, you must have a properly configured PC and a properly configured instrument, as described in the following table.
|
Instruments |
Requirements |
|---|---|
|
N5172B EXG X-Series RF vector signal generator |
Firmware: Version B.01.10 or later (how to upgrade) Version B.01.20 or later for real time software Required options: N5172B-503 (9 kHz to 3 GHz frequency range) N5172B-653 (Internal baseband generator, 32 MSa/sec, up to 60 MHz RF bandwidth) N5172B-660 (upgrade baseband generator with real-time capability) Recommended options: N5172B-009 (internal Flash drive) N5172B-021 (upgrade baseband generator memory from 32 MSa to 256 MSa) N5172B-1EA (high power output for PA testing) N5172B-1ER (flexible reference input, 1-50 MHz) N5172B-403 (calibrated AWGN for testing with noise) N5172B-655 (upgrade baseband generator from 60 to 120 MHz RF bandwidth) N5172B-UNV (enhanced dynamic range) N5172B-UNZ (fast switching for manufacturing environments) |
|
N5182B MXG X-Series RF vector signal generator |
Firmware: Version B.01.10 or later (how to upgrade) Version B.01.20 or later for real time software Required options: N5182B-503 (9 kHz to 3 GHz frequency range) N5182B-656 (Internal baseband generator, 32 MSa/sec, up to 80 MHz RF bandwidth) N5182B-660 (upgrade baseband generator with real-time capability) Recommended options: N5182B-009 (internal Flash drive) N5182B-022 (upgrade baseband generator memory from 32 MSa to 512 MSa) N5182B-1EA (high power output for PA testing) N5182B-1ER (flexible reference input, 1-50 MHz) N5182B-1EQ (low power output for Rx testing) N5182B-403 (calibrated AWGN for testing with noise) N5182B-657 (upgrade baseband generator from 80 to 160 MHz RF bandwidth) N5182B-UNV (enhanced dynamic range) N5182B-UNZ (fast switching for manufacturing environments) |
|
N5182A MXG vector signal generator (For more information see the Configuration Guide) |
Firmware: Version A.01.51 or later (how to upgrade) Required options: One of the following baseband generator options:
Additional options to consider:
|
|
E4438C ESG vector signal generator (For more information see the Configuration Guide) |
Firmware: Version C.05.24 or later (how to upgrade) Required options: One of the following baseband generator options:
Additional options to consider:
|
|
E8267D PSG vector signal generator (For more information see the Configuration Guide) |
Firmware: Version C.04.85 or later (how to upgrade) Required options: One of the following baseband generator options:
Additional options to consider:
|
|
N5106A PXB baseband generator and channel emulator |
Required options:
|
|
M9381A PXIe vector signal generator |
Driver: Version 1.4.400.0 or later Recommended options: M9381A-M05 (memory 512 MSa) M9381A-M10 (memory 1024 MSa) M9381A-1EA (high output power) M9381A-B10 (RF modulation bandwidth 100 MHz) M9381A-B16 (RF modulation bandwidth 160 MHz) Additional options to consider: M9381A-F06 (frequency range 1 MHz to 6 GHz) Limitations: The M9381A VSG has a limitation related to the Power Search and DC Cal functions, creating a time-synchronization loss. That is, the signal timing changes after a Power Search or DC Cal. When ALC is set to Off, Signal Studio automatically runs Power Search, which affects the user's trigger signal for starting waveform playback. Even though the timing alignment of the trigger signal and waveform are properly set, the Power Search function disrupts this synchronization. In these cases, use the following workarounds:
For DC Cal, run it before you download and play the waveform. Do not run DC Cal while the signal is playing, which disrupts the synchronization. |
|
E6640A EXM wireless test set |
Software: Version E.16.06 or later Recommended options: E6640A-B85 (increases signal bandwidth to 80 MHz) E6640A-B1X (increases signal bandwidth to 160 MHz) Y-Options (these option models, beginning with "Y," combine signal creation and measurement applications) Additional options to consider: E6640A-506 (380 MHz to 6 GHz frequency range) E6640A-5WC (frequency range for wireless connectivity) |
|
E6650A EXF wireless test set for femtocell |
Software: Version F.16.06 or later Recommended options: E6650A-B85 (increases signal bandwidth to 80 MHz) E6650A-B1X (increases signal bandwidth to 160 MHz) Y-Options (these option models, beginning with "Y," combine signal creation and measurement applications) Additional options to consider: E6650A-506 (380 MHz to 6 GHz frequency range) E6650A-5WC (frequency range for wireless connectivity) |
|
M9420A VXT PXIe vector transceiver |
Software: Version M.16 or later Recommended options: M9420A-1EA (high output power) M9420A-B85 (increases signal bandwidth to 80 MHz) M9420A-B1X (increases signal bandwidth to 160 MHz) M9420A-M05 (memory 512 MSa) Additional options to consider: M9420A-506 (frequency range 6 GHz) M9420A-FDX (full duplex ports) M9420A-HDX (half duplex ports) |
200 GB HDD with 2 GB free disk space at runtime (5 GB or higher recommended)
1024 x 768 screen resolution (1280 x 1024 recommended)
Windows 8.1 (Pro/Enterprise) (32/64 bit)1,2:
1 GHz or faster 32-bit or 64-bit processor
1 GB of memory minimum for the 32-bit version
2 GB of memory minimum for a 64-bit version
1.5 GB hard disk space (includes 1 GB for Microsoft .NET Framework and 65 MB for the Keysight IO Libraries)
Microsoft Internet Explorer (8.0 or later)
Microsoft .NET Framework 3.5 or .NET Framework 3.5 Service Pack 1 (See "2. Downloading and Installing the .NET Framework")
Keysight IO Libraries, version 17.1 or later (See "3. Downloading and Installing the Keysight IO Libraries Suite")
Keysight License Manager (See "4. Downloading and Installing the Keysight License Manager ")
128 MB graphics memory with DirectX 9 graphics support (recommended)
Windows 7 (Professional/Ultimate/Enterprise)1,2:
1 GHz or faster 32-bit or 64-bit processor
1 GB of memory minimum for the 32-bit version
2 GB of memory minimum for a 64-bit version
1.5 GB hard disk space (includes 1 GB for Microsoft .NET Framework and 65 MB for the Keysight IO Libraries)
Microsoft Internet Explorer (8.0 or later)
Microsoft .NET Framework 3.5 or .NET Framework 3.5 Service Pack 1 (included with Windows 7) (See "2. Downloading and Installing the .NET Framework")
Keysight IO Libraries, version 17.1 or later (See "3. Downloading and Installing the Keysight IO Libraries Suite")
Keysight License Manager (See "4. Downloading and Installing the Keysight License Manager ")
128 MB graphics memory with DirectX 9 graphics support (recommended)
Installed GPIB IO interface card, LAN interface card, or USB/GPIB interface connector
Keysight VISA
Microsoft Windows Installer version 2.0 or later
1 No support for Itanium64.
2 Signal Studio is compatible with the 64-bit operating system, but performs at the 32-bit speed.