The code domain power (CDP) graph shows the position and power level
of each downlink
channel or uplink
channel, relative to the spreading code applied. Select a channel setup
in the
tree view
then click the CDP tab to view the CDP distribution for that carrier.
Click on a channel in the channel configuration summary table or double-click
a channel in the graph to view the
parameter
selections
for that channel.
Hold the cursor over any individual channel to view a
tool tip
showing the channel number, type, spreading code, rate, and power.